This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccsv5 on linux, hardware trace analyzer problem

Hi,

I'm running ccsv5.5 on linux and trying to run tools->hardware trace analyzer->PC trace. My setup is xds560v2 with pandaboard (omap4430 es2.1). The problem is that after I clicked the "start" in the PC trace configuration dialog, it poped out an error saying "Could not run analyzer on CortexA9_0. Cause: unable to select receiver". I didn't changed any default settings. I used the default .ccxml target configuration file for pandaboard. It has a CSETB_0 device at address 0x54162000, with TraceDeviceId 0x0, and with NO initialization script.

Please help! Thank you.