Other Parts Discussed in Thread: MSP430F5438A
I have a few projects that were built in either CCE v3, CCS v4, and now CCS v5. I just recently opened a project in
Version: CCE v3.1 Build: 3.2.4.3.8
and cannot connect my USB-FET. That is, when I debug, I get the error: no USB FET found. But, it shows as a connected device in device manager.
So, I figure the FW version is not correct and I downgrade to MSP-FET430UIF FW version 2.04.09.001. Now when I try to debug, I get an error: Version mismatch, a firmware update is required.
But, whenever I update, it always says it can't be found.
What version of FW for the USB-FET do I need in order to debug my CCE v3.1 project? Any drivers I need to be aware of? I'd like to get this USB-FET configured correctly for CCE v3.1 and have it labeled as such. I believe I accidently updated the version when I debugged a CCS v5 project.
Thanks