All:
I am using CCS 5.5, and I was unsuccessful at migrating an existing project from CCS 3.3 to CCS 5.5 - I have been advised to create a new project. However, when I try creating a new project, C6713 is not an option under DSP/BIOS. I tried using C6748, but that did not let me easily create the DSP/BIOS stuff.
Is there a good starting point when starting from scratch? (a particular processor??)
Possible options from the DSP/BIOS v5.xx Examples:
dsk6416 Examples
dsk6455 Examples
evm6424 Examples
evm6474 Examples
... etc.