This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't build projects in ControlSuite

Other Parts Discussed in Thread: CONTROLSUITE

Hi TI E2E.

I am using CCS v5.5 and the latest version of controlSuite. I realised that most of examples in it can't not be built without doing something and most of example projects in folders in Development Tool folder such as Motor, Digital power ... cant be built with my knowlegde.

Please help me to solve that problem.

Such as when I build example for High Voltage Interleaved PFC kit after clicking in the link to import it:

Description Resource Path Location Type
unresolved symbol _FlashRegs, first referenced in ./ILPFC-DevInit_F2803x.obj ILPFC C/C++ Problem
unresolved symbol _GpioCtrlRegs, first referenced in ./ILPFC-DevInit_F2803x.obj ILPFC C/C++ Problem
unresolved symbol _EPwm6Regs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _EPwm7Regs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _PieVectTable, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _SCIA_Init, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _GpioDataRegs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _PieCtrlRegs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol __IQ15div, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol __IQ15isqrt, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _SerialHostComms, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
errors encountered during linking; "ILFC_2803x.out" not built ILPFC C/C++ Problem
unresolved symbol _SysCtrlRegs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol __IQ15sqrt, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbols remain ILPFC C/C++ Problem
unresolved symbol __IQ15rmpy, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol __IQ15rsmpy, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _AdcResult, first referenced in ./ILPFC-DPL-ISR.obj ILPFC C/C++ Problem
unresolved symbol _AdcRegs, first referenced in ./DSP2803x_Adc.obj ILPFC C/C++ Problem
unresolved symbol _ADC_SOC_CNF, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _CpuTimer0Regs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _Comp3Regs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _Comp2Regs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _Comp1Regs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _EPwm1Regs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _DSP28x_usDelay, first referenced in ./DSP2803x_Adc.obj ILPFC C/C++ Problem
unresolved symbol _CpuTimer2Regs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _CpuTimer1Regs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _EPwm5Regs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _EPwm4Regs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _EPwm3Regs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem
unresolved symbol _EPwm2Regs, first referenced in ./ILPFC-Main.obj ILPFC C/C++ Problem

Same problem with High Voltage Power Factor Correction kit example:

Description Resource Path Location Type
unresolved symbols remain PFC2PhiL-Main.c /PFC2PhiL C/C++ Problem
errors encountered during linking; "PFC2PhiL.out" not built PFC2PhiL-Main.c /PFC2PhiL C/C++ Problem
unresolved symbol _Comp2Regs, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem
unresolved symbol _Comp1Regs, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem
unresolved symbol _AdcResult, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem
unresolved symbol _ADC_SOC_CNF, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem
program will not fit into F28027_RAM_PFC2PHIL.CMD /PFC2PhiL line 90 C/C++ Problem
unresolved symbol _CpuTimer0Regs, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem
unresolved symbol _CpuTimer1Regs, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem
unresolved symbol _CpuTimer2Regs, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem
unresolved symbol _EPwm1Regs, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem
unresolved symbol _EPwm2Regs, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem
unresolved symbol _EPwm3Regs, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem
unresolved symbol _EPwm4Regs, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem
unresolved symbol _FlashRegs, first referenced in ./PFC2PHIL-DevInit_F2802x.obj PFC2PhiL C/C++ Problem
unresolved symbol _GpioCtrlRegs, first referenced in ./PFC2PHIL-DevInit_F2802x.obj PFC2PhiL C/C++ Problem
unresolved symbol _PWM_PFC2PHIL_CNF, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem
unresolved symbol _PieCtrlRegs, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem
unresolved symbol _PieVectTable, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem
unresolved symbol _SysCtrlRegs, first referenced in ./PFC2PhiL-Main.obj PFC2PhiL C/C++ Problem

Thank you.

  • The root cause of this problem is in some error in project configuration.  I lack expertise in how controlSuite projects are typically configured.

    But I do have one suggestion which may help.  When you import the project into CCS, try checking the box Copy projects into workspace.  There is a chance some library or link command file needs to be copied from the controlSuite area into the workspace to make everything work.  If this doesn't work out, then I need to move this thread to the C2000 forum.

    Thanks and regards,

    -George

  • Hi Tan!

    Try to do the following.

    Regarding your Project #1

    1 Check "Include options" of project's properties

    C:\ti\controlSUITE\device_support\f2803x\v127\DSP2803x_common\include\

    C:\ti\controlSUITE\device_support\f2803x\v127\DSP2803x_headers\include\

    C:\ti\controlSUITE\libs\math\IQmath\v15c\include\

    2 Add into your project folder file  DSP2803x_GlobalVariableDefs.c  from

    C:\ti\controlSUITE\device_support\f2803x\v127\DSP2803x_headers\source\

    Regarding your Project#2

    1 Check "Include options" of project's properties

    C:\ti\controlSUITE\device_support\f2802x\v210\f2802x_common\include\

    C:\ti\controlSUITE\device_support\f2802x\v210\f2802x_headers\include\

    2 Add into your project folder file  DSP2802x_GlobalVariableDefs.c  from

    C:\ti\controlSUITE\device_support\f2802x\v210\f2802x_headers\source\

    Regards,

    Igor