Other Parts Discussed in Thread: TMS320F28335
Hi,
I've made a few XDS100V2 Emulator boards based on the design details provided by the TI.When I try to load program into TMS320F28335 by one of these emulators i am getting an error message which says "Device is in low power mode,Do you want to bring it out of this mode" for which i've selected YES but not working. With other XDS100V2 emulator it is working fine.
I am using CCSV5.4 and used Test Connection option to check the faulty emulator. It reports some operations are failed and in the summary it is said that 83% failed.Other XDS100v2 emulators are tested success.
Any suggestion where the problem lies ?