In CCSV3.3 , there is a project file .prj containing the info. about the source files within the project, compiler options, build options, etc.. Is there a correcponding file in CCSV5? Since I need to archieve the project, so other people can regenerate the .out file on their computer. There are few folders and files generated within workspace. I believe I do not need to archieve everything within the workspace. Can you advice which file(s)/folder should I archieve to keep the project integrity.
Thanks
Honghui