Hi,
CCS5.5 installation failed several times. My system is win8.
I have disabled the McAfee but no success.
Could anyone give me a hand? Thanks.
here is my installation log.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
CCS5.5 installation failed several times. My system is win8.
I have disabled the McAfee but no success.
Could anyone give me a hand? Thanks.
here is my installation log.
Hi Hyde, (Hi Igor)
The above steps should solve your issue; if still you face any issue try downloading the CCS v5.5 setup.exe again.
Regards,
Gautam
Hi Hyde,
are you using a VM type setup at all? I ask because I see two drives involved in the installation. Sometimes this causes problems is there is a permissions/antivirus issue between the two or else a connection problem.
Would you be able to clear out all your attempts, including the logs and try again all in one drive? Ie all in C:?
Please keep us informed.
Best Regards,
Lisa
Sorry, I forgot to update my condition.
The installation of CCS5.5 is successful.
I indeed used virtual machine. However, even though I removed it and logs, the installation is still failed.
I think that it was perhaps related to my os (win8, 64bit). Because when I installed CCS5.5 in virtual machine(win xp,32bit), the installation suceeded .