Other Parts Discussed in Thread: MOTORWARE, TMS320F28035
Hi,
I was forced to switch computers and decided to upgrade from CCS 4 to latest CC5.
I'm working with DRV8312EVM Rev D.
And now I cannot connect to target.
After installing CCS v5 I imported all the example projects:
C:\ti\motorware\motorware_1_01_00_10\sw\solutions\instaspin_foc\boards\drv8312kit_revD\f28x\f2806xF\projects\ccs5\*
and I created a new Target in Target Configurations view:
- Connection:Texas Instruments XDS100v1 USB Emulator
- Board or Device: TMS320F28035
I then open the Debug view and see:
Texas Instruments XDS100v1 USB Emulator_0/C28xx (Disconnected : Unknown) Texas Instruments XDS100v1 USB Emulator_0/CLA_0 (Disconnected : Unknown)
Texas Instruments XDS100v1 USB Emulator_0/C28xx (Disconnected : Unknown)
Texas Instruments XDS100v1 USB Emulator_0/CLA_0 (Disconnected : Unknown)
I right click on the C28xx line and select Connect from the popup menu and I get this error:
C28xx: Error connecting to the target: (Error -1135 @ 0x0) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.232.0)
I go to the Windows (7) Device Manager and I see that board is connected as:
Texas Instruments XDS100+RS232 V1.0/properties/Hardware
TI XDS100 Channel A
TI XDS100 Channel B
USB Composite Device
USB Serial Port (COM12)
Device is working properly
So any ideas how to proceed to find out what am I doing wrong?
Dejavualloveragain .... I think I was in this spot half a year ago.
br Kusti
PS why the example projects is/has f2806xF and 2806xF but no f28035?