Other Parts Discussed in Thread: MSP430F2013
Hello,
I bought a eZ430-F2013 few days ago and installed it on 2 PCs. On the first PC all is OK. On the second one the following error message appears when launching "debug active Project" in CCE.
Exception occured during launch
Reason: Failed to initialize the Debug Server
Reason: System Setup XML File: C:/.../TargetDB/MSP430F2013_TIMSP430-USB.xml contains invalid characters: 'e
History of the installation:
1/ installed CCS V4
2/ installed "eZ430-F2013" hardware
--> then CCS reported the error above
3/ uninstalled CCS V4
4/ installed CCE V3.1
--> then CCE reported same error above
I had a look at the XML file specified in the error message and didn't find the 'e character that seems to create the error.
In the Device manager, I can see the "Port (COM LPT)" > "MSP-FET430UIF-VCP(COM10)" so apparently the hardware installation is OK.
I'm beginner with CCE and MSP430. Do you have any idea of what could be the root cause of this issue.
Thanks in advance for your help.
Chris