Other Parts Discussed in Thread: TCI6638K2K, UNIFLASH
Hi All,
We have recently received TCI6638EVMK2X board from TI. I could able to access the consoles(both TCI6638 and BMC) from Teraterm. But I couldnot able to connect to the target board from my CCSv5.4. I am getting below error with Test Connection.
-----------------------------------------------------------------------------------------------------------------
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -r -o -S pathlength -S integrity
[Result]
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_io
Failed to open i/o connection (xds2xxu:0)
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the named emulator via USCIF ECOM has failed.
[End]
-----------------------------------------------------------------------------------------------------------------
As per the user guide, I have chosen the correct target configuration, TI XDS2xx USB Emulator_0->TCI6638K2K and loaded xtcievmk2x GEL file. I have configured the board in JTAG mode but could not able to make a connection with target from CCS.
I have tried with other configurations, modes and GEL files but I get the same above error always. Could anyone help me solving this issue? Are there any points I am missing or to lookout for?
Thanks
kg