This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Errors Loading CCv5 since Windows 8.1 update

I have had the 3 errors below since I updated to from Windows 8.0 to Windows 8.1 not sure how to fix:

An internal error occurred during: "CrashTrackerJob". C:\ti\ccsv5\ccs_base\DebugServer\bin\LibraryLoader.dll: Can't find dependent libraries

An internal error occurred during: "License Acquisition". C:\ti\ccsv5\ccs_base\DebugServer\bin\ti_xpcom.dll: Can't find dependent libraries

An internal error occurred during: "Loading device information". C:\ti\ccsv5\ccs_base\common\bin\fsutiljni.dll: Can't find dependent libraries

  • Hi Gavin,

    do you get any error logs (hs_err____.log fies) or dump files (.dmp)?   If you are crashing at startup, perhaps not.   There are a few things you can try in between

    - a fresh workspace (again maybe not possible)

    - run the vcredist*.exe package in the ccs folders to see if restoring the visual c redistributable does the trick.  The update could well have changed something there

    - look at the wiki below

    http://processors.wiki.ti.com/index.php/Troubleshooting_CCS

    Please keep us informed.

    Best regards,
    Lisa 

  • I tried all those options before, and I've seen the wiki... 

    My initially problem was CCSv5 would freeze and stop responding while starting up, directly after you choose the workspace you wanted to work in:

    • I got pass the initial issue by deleting the .metadata folder that was in the workspace I was trying to use
    But since I got pass that intially issue I'm getting these new errors and I haven't seen anything on the boards about them.
  • Gavin,

    From what you describe, my suspicion is the Windows 8.1 update somehow change the availability of previously installed Microsoft runtime libraries.  Could you try re-running these three Microsoft installers to see if it helps: VS2005, VS2008, VS2012 .  Please let us know what happens.

  • Thanks re-running those 3 Microsoft installers did the trick.

  • Thank you for this post.  I ran into the same problem, and the answers here pointed me in the right direction.  I had to uninstall the Microsoft VS redistributables and then reinstall them.  Then the issue went away.

  • I have notebook with Windows 7.

    Many day everythings  with CCS v5 was very good.

    Now during open the CCS v5 I got Notice:

    An internal error occurred during: "License Acquisition".

    java.lang.NullPointerException

    What is the error ?

    Can You help me?

    The best regards.

  • I suggest you remove all of the VS redistributables on your computer and then re-run the CCSv5 installer.  That worked for me.

  • I have had the 3 errors below since I updated to from ccs5.3 to 5.4 not sure how to fix:

    An internal error occurred during: "CrashTrackerJob".C:\ti\ccsv5\ccs_base\DebugServer\bin\LibraryLoader.dll: %1 is not a valid Win32 application
    An internal error occurred during: "License Acquisition".C:\ti\ccsv5\ccs_base\DebugServer\bin\ti_xpcom.dll: Can't find dependent libraries
    An internal error occurred during: "Loading device information". C:\ti\ccsv5\ccs_base\common\bin\fsutiljni.dll: Can't find dependent libraries

    I have delete all the installation from PC related to ccs and reinstall it.
    Also try the above one,but still geeting the same error.
    Can You help me?
  • I have had the 3 errors below since I updated to from ccs5.3 to 5.4 not sure how to fix:

    An internal error occurred during: "CrashTrackerJob".C:\ti\ccsv5\ccs_base\DebugServer\bin\LibraryLoader.dll: %1 is not a valid Win32 application
    An internal error occurred during: "License Acquisition".C:\ti\ccsv5\ccs_base\DebugServer\bin\ti_xpcom.dll: Can't find dependent libraries
    An internal error occurred during: "Loading device information". C:\ti\ccsv5\ccs_base\common\bin\fsutiljni.dll: Can't find dependent libraries

    I have delete all the installation from PC related to ccs and reinstall it.
    Also try the above one,but still geeting the same error.
    Can You help me?
  • For me, uninstalling CCS was not enough. I had to actually go into the Windows Add/Remove Programs area and remove all versions of the Microsoft VS Redistributable packages. Then I reinstalled CCS, and it worked. If that doesn't work for you, I don't know what the issue is.
  • CCS 5.4 depends on the newer 2012 MS redistributable, whereas CCS 5.3 did not.  Most likely that redistributable was not installed on your machine.  Please download and install it from the link provided above.

    Darian

  • I have vcredist_x86_2012 ms  redistributable is installed while while install the tool, but its not working.

    Should I install vcredist_x64_2012 also?

  • I have removed all the CSS folder from C drive and also remove all the installed tools from add/remove window.but still same problem.
  • If you are still seeing the above error loading LibraryLoader.dll after installing the redistributable, please download and run dependency walker (http://www.dependencywalker.com/depends22_x86.zip), start it, drag LibraryLoader.dll on top of it (from ccsv5\ccs_base\DebugServer\bin), save it as text and attach it to this thread.

    Darian

  • Hello Darian,

    Should I run _x86 or _x64 , because I have window 7 with 64 bit os?

    And I have 3 dll error.Shoul I run this for all 3 dll.

    LibraryLoader.txt

  • Hello Darian,

    Thanks for your suggestion.
    What a tool is "dependencywalker".
    This tools identify which file is corropted or missing in the system.
    I load LibraryLoader.dll file and get that which file having problem.
    The problem is with msvcr110.dll file which is related to visual c++ redistributable and was missing in C:\Windows\System32 path of pc.
    Then I used dll file fixer to fix the problem.
    Now its working fine for me.
    Before all this stuff if your system is 64 bit OS then install both redistributable, like vcredist_x86_2012 and vcredist_x64_2012.

    Thanks a lot again.
  • Krushna,

    For the error you were having, you should just need the x86 redistributable (as libraryloader.dll is a 32 bit dll).  However, installing both won't hurt.  I'm glad it's working for you now.

    Darian

  • Hello , i am also facing same problem as described earlier in blog.

    As a solution i found that , I should uninstall all MSVC and reinstall 2005 and 2012 32-bit.

    I tried that and then I tried to reinstall CCS but the error still exist.

    Now i found your suggestion to attach .txt file.So i am attaching that,Please find it and give me solution of this issue.

    By using dependencywalker software i able to find that 2 DLL files were missing.I downloaded them and put it in SYSWOW64 folder as mine laptop is x64bit. But that also couldn't solve errors.

    So please suggest me what should i do?

    Thanks.

    *****************************| System Information |*****************************
    
    Dependency Walker:       2.2.6000 (32-bit)
    Operating System:        Microsoft Windows NT/2000/XP/2003/Vista based Professional (64-bit)
    OS Version:              6.02.9200
    Processor:               Intel64 Family 6 Model 58 Stepping 9, GenuineIntel, ~1796MHz
    Number of Processors:    2, Mask: 0x00000003
    Computer Name:           DHRUVIL
    User Name:               User
    Local Date:              17 December 2016
    Local Time:              12:41:24 AM India Standard Time (GMT+05:30)
    OS Language:             0x4009: Unknown
    Memory Load:             63%
    Physical Memory Total:   4,170,473,472 (3978 MB)
    Physical Memory Used:    2,666,393,600
    Physical Memory Free:    1,504,079,872
    Page File Memory Total:  4,294,967,295
    Page File Memory Used:   1,343,238,143
    Page File Memory Free:   2,951,729,152
    Virtual Memory Total:    2,147,352,576
    Virtual Memory Used:     162,541,568
    Virtual Memory Free:     1,984,811,008
    Page Size:               0x00001000 (4,096)
    Allocation Granularity:  0x00010000 (65,536)
    Min. App. Address:       0x00010000 (65,536)
    Max. App. Address:       0x7FFEFFFF (2,147,418,111)
    
    ********************************| Search Order |********************************
    *                                                                              *
    * Legend: F  File                     E  Error (path not valid)                *
    *                                                                              *
    ********************************************************************************
    
    Side-by-Side components (Windows 2000/XP/2003/Vista/+)
    The system's "KnownDLLs" list
       [F ] c:\windows\system32\ADVAPI32.DLL
       [F ] c:\windows\system32\CFGMGR32.DLL
       [F ] c:\windows\system32\CLBCATQ.DLL
       [F ] c:\windows\system32\COMBASE.DLL
       [F ] c:\windows\system32\COMCTL32.DLL
       [F ] c:\windows\system32\COMDLG32.DLL
       [F ] c:\windows\system32\CRYPT32.DLL
       [F ] c:\windows\system32\DIFXAPI.DLL
       [F ] c:\windows\system32\GDI32.DLL
       [F ] c:\windows\system32\GDIPLUS.DLL
       [F ] c:\windows\system32\IMAGEHLP.DLL
       [F ] c:\windows\system32\IMM32.DLL
       [F ] c:\windows\system32\KERNEL32.DLL
       [F ] c:\windows\system32\KERNELBASE.DLL
       [F ] c:\windows\system32\LPK.DLL
       [F ] c:\windows\system32\MSASN1.DLL
       [F ] c:\windows\system32\MSCTF.DLL
       [F ] c:\windows\system32\MSVCRT.DLL
       [F ] c:\windows\system32\NORMALIZ.DLL
       [F ] c:\windows\system32\NSI.DLL
       [F ] c:\windows\system32\NTDLL.DLL
       [F ] c:\windows\system32\NTDLL.DLL
       [F ] c:\windows\system32\OLE32.DLL
       [F ] c:\windows\system32\OLEAUT32.DLL
       [F ] c:\windows\system32\PSAPI.DLL
       [F ] c:\windows\system32\RPCRT4.DLL
       [F ] c:\windows\system32\SECHOST.DLL
       [F ] c:\windows\system32\SETUPAPI.DLL
       [F ] c:\windows\system32\SHELL32.DLL
       [F ] c:\windows\system32\SHLWAPI.DLL
       [F ] c:\windows\system32\USER32.DLL
       [F ] c:\windows\system32\WINTRUST.DLL
       [F ] c:\windows\system32\WLDAP32.DLL
       [F ] c:\windows\system32\WOW64.DLL
       [F ] c:\windows\system32\WOW64CPU.DLL
       [F ] c:\windows\system32\WOW64WIN.DLL
       [F ] c:\windows\system32\WS2_32.DLL
    The application directory
       [  ] C:\ti\ccsv6\ccs_base\DebugServer\bin\
    The 32-bit system directory
       [  ] C:\Windows\system32\
    The 16-bit system directory (Windows NT/2000/XP/2003/Vista/+)
       [  ] C:\Windows\system\
    The system's root OS directory
       [  ] C:\Windows\
    The application's registered "App Paths" directories
    The system's "PATH" environment variable directories
       [  ] C:\Program Files (x86)\NVIDIA Corporation\PhysX\Common\
       [  ] C:\Windows\system32\
       [  ] C:\Windows\
       [  ] C:\Windows\System32\Wbem\
       [  ] C:\Windows\System32\WindowsPowerShell\v1.0\
       [  ] C:\Program Files (x86)\Windows Live\Shared\
       [  ] C:\Program Files (x86)\MATLAB\R2008b\bin\
       [  ] C:\Program Files (x86)\MATLAB\R2008b\bin\win32\
       [  ] C:\Program Files (x86)\Skype\Phone\
       [  ] C:\TDM\bin\
    
    ***************************| Module Dependency Tree |***************************
    *                                                                              *
    * Legend: F  Forwarded Module   ?  Missing Module        6  64-bit Module      *
    *         D  Delay Load Module  !  Invalid Module                              *
    *         *  Dynamic Module     E  Import/Export Mismatch or Load Failure      *
    *                               ^  Duplicate Module                            *
    *                                                                              *
    ********************************************************************************
    
    [   ] LIBRARYLOADER.DLL
         [   ] KERNEL32.DLL
              [   ] API-MS-WIN-CORE-RTLSUPPORT-L1-2-0.DLL
              [   ] NTDLL.DLL
              [   ] KERNELBASE.DLL
                   [ ^ ] NTDLL.DLL
                   [D  ] EXT-MS-WIN-ADVAPI32-REGISTRY-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-KERNEL32-APPCOMPAT-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-NTUSER-STRING-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-KERNEL32-FILE-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-KERNEL32-DATETIME-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-KERNEL32-QUIRKS-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-KERNEL32-SIDEBYSIDE-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-MRMCORER-RESMANAGER-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-KERNEL32-WINDOWSERRORREPORTING-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-GPAPI-GROUPPOLICY-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-NTDSAPI-ACTIVEDIRECTORYCLIENT-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-SHELL32-SHELLCOM-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-SHELL32-SHELLFOLDERS-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-ADVAPI32-NTMARTA-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-KERNEL32-ERRORHANDLING-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-KERNEL32-REGISTRY-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-KERNELBASE-PROCESSTHREAD-L1-1-0.DLL
                   [D  ] EXT-MS-WIN-APPXDEPLOYMENTCLIENT-APPXDEPLOY-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-PROCESSTHREADS-L1-1-2.DLL
              [   ] API-MS-WIN-CORE-REGISTRY-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-HEAP-L1-2-0.DLL
              [   ] API-MS-WIN-CORE-MEMORY-L1-1-2.DLL
              [   ] API-MS-WIN-CORE-HANDLE-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-SYNCH-L1-2-0.DLL
              [   ] API-MS-WIN-CORE-FILE-L1-2-1.DLL
              [   ] API-MS-WIN-CORE-DELAYLOAD-L1-1-1.DLL
              [   ] API-MS-WIN-CORE-IO-L1-1-1.DLL
              [   ] API-MS-WIN-CORE-JOB-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-THREADPOOL-LEGACY-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-THREADPOOL-PRIVATE-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-LIBRARYLOADER-L1-2-0.DLL
              [   ] API-MS-WIN-CORE-NAMEDPIPE-L1-2-0.DLL
              [   ] API-MS-WIN-CORE-DATETIME-L1-1-1.DLL
              [   ] API-MS-WIN-CORE-SYSINFO-L1-2-1.DLL
              [   ] API-MS-WIN-CORE-TIMEZONE-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-LOCALIZATION-L1-2-1.DLL
              [   ] API-MS-WIN-CORE-LOCALIZATION-PRIVATE-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-PROCESSENVIRONMENT-L1-2-0.DLL
              [   ] API-MS-WIN-CORE-STRING-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-DEBUG-L1-1-1.DLL
              [   ] API-MS-WIN-CORE-ERRORHANDLING-L1-1-1.DLL
              [   ] API-MS-WIN-CORE-FIBERS-L1-1-1.DLL
              [   ] API-MS-WIN-CORE-UTIL-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-PROFILE-L1-1-0.DLL
              [   ] API-MS-WIN-SECURITY-BASE-L1-2-0.DLL
              [   ] API-MS-WIN-CORE-COMM-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-WOW64-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-REALTIME-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-SYSTEMTOPOLOGY-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-PROCESSTOPOLOGY-L1-2-0.DLL
              [   ] API-MS-WIN-CORE-NAMESPACE-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-FILE-L2-1-1.DLL
              [   ] API-MS-WIN-CORE-XSTATE-L2-1-0.DLL
              [   ] API-MS-WIN-CORE-LOCALIZATION-L2-1-0.DLL
              [   ] API-MS-WIN-CORE-NORMALIZATION-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-SIDEBYSIDE-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-APPCOMPAT-L1-1-1.DLL
              [   ] API-MS-WIN-CORE-WINDOWSERRORREPORTING-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-CONSOLE-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-CONSOLE-L2-1-0.DLL
              [   ] API-MS-WIN-CORE-PSAPI-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-PSAPI-ANSI-L1-1-0.DLL
              [   ] API-MS-WIN-CORE-PSAPI-OBSOLETE-L1-1-0.DLL
              [   ] API-MS-WIN-SECURITY-APPCONTAINER-L1-1-0.DLL
              [F^ ] NTDLL.DLL
         [ ? ] MSVCP140.DLL
         [ ? ] VCRUNTIME140.DLL
         [   ] API-MS-WIN-CRT-ENVIRONMENT-L1-1-0.DLL
              [F  ] UCRTBASE.DLL
                   [ ^ ] API-MS-WIN-CORE-STRING-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-ERRORHANDLING-L1-1-0.DLL
                   [ ^ ] API-MS-WIN-CORE-TIMEZONE-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-FILE-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-NAMEDPIPE-L1-1-0.DLL
                   [ ^ ] API-MS-WIN-CORE-HANDLE-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-FILE-L2-1-0.DLL
                   [   ] API-MS-WIN-CORE-HEAP-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-LIBRARYLOADER-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-SYNCH-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-PROCESSTHREADS-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-PROCESSENVIRONMENT-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-DATETIME-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-LOCALIZATION-L1-2-0.DLL
                   [   ] API-MS-WIN-CORE-SYSINFO-L1-1-0.DLL
                   [ ^ ] API-MS-WIN-CORE-SYNCH-L1-2-0.DLL
                   [ ^ ] API-MS-WIN-CORE-CONSOLE-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-DEBUG-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-PROCESSTHREADS-L1-1-1.DLL
                   [   ] API-MS-WIN-CORE-FILE-L1-2-0.DLL
                   [ ^ ] API-MS-WIN-CORE-PROFILE-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-MEMORY-L1-1-0.DLL
                   [ ^ ] API-MS-WIN-CORE-UTIL-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-RTLSUPPORT-L1-1-0.DLL
                   [   ] API-MS-WIN-CORE-INTERLOCKED-L1-1-0.DLL
         [   ] API-MS-WIN-CRT-RUNTIME-L1-1-0.DLL
              [F^ ] UCRTBASE.DLL
         [   ] API-MS-WIN-CRT-HEAP-L1-1-0.DLL
              [F^ ] UCRTBASE.DLL
    
    ********************************| Module List |*********************************
    *                                                                              *
    * Legend: D  Delay Load Module   ?  Missing Module           6  64-bit Module  *
    *         *  Dynamic Module      !  Invalid Module                             *
    *                                E  Import/Export Mismatch or Load Failure     *
    *                                                                              *
    ********************************************************************************
    
           Module                                                 File Time Stamp    Link Time Stamp    File Size  Attr.  Link Checksum  Real Checksum  CPU  Subsystem  Symbols     Preferred Base  Actual Base  Virtual Size  Load Order  File Ver          Product Ver       Image Ver  Linker Ver  OS Ver  Subsystem Ver
    -----  -----------------------------------------------------  -----------------  -----------------  ---------  -----  -------------  -------------  ---  ---------  ----------  --------------  -----------  ------------  ----------  ----------------  ----------------  ---------  ----------  ------  -------------
    [ ? ]  MSVCP140.DLL                                           Error opening file. The system cannot find the file specified (2).
    [ ? ]  VCRUNTIME140.DLL                                       Error opening file. The system cannot find the file specified (2).
    [   ]  API-MS-WIN-CORE-APPCOMPAT-L1-1-1.DLL                   22-08-2013 09:47a  22-08-2013 09:47a      3,584  HA     0x00007682     0x00007682     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-COMM-L1-1-0.DLL                        22-08-2013 09:44a  22-08-2013 09:44a      3,584  HA     0x0000EAEF     0x0000EAEF     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-CONSOLE-L1-1-0.DLL                     22-08-2013 09:44a  22-08-2013 09:44a      3,584  HA     0x000090A4     0x000090A4     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-CONSOLE-L2-1-0.DLL                     22-08-2013 09:44a  22-08-2013 09:44a      4,096  HA     0x00001528     0x00001528     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-DATETIME-L1-1-0.DLL                    22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x0000B1AC     0x0000B1AC     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-DATETIME-L1-1-1.DLL                    22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x000019CB     0x000019CB     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-DEBUG-L1-1-0.DLL                       22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x000099B5     0x000099B5     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-DEBUG-L1-1-1.DLL                       22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x00005CFC     0x00005CFC     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-DELAYLOAD-L1-1-1.DLL                   22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x00007C0D     0x00007C0D     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-ERRORHANDLING-L1-1-0.DLL               22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x0000AAC3     0x0000AAC3     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-ERRORHANDLING-L1-1-1.DLL               22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x0000577D     0x0000577D     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-FIBERS-L1-1-1.DLL                      22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x000104C0     0x000104C0     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-FILE-L1-1-0.DLL                        22-08-2013 09:47a  22-08-2013 09:47a      4,608  HA     0x00006C05     0x00006C05     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-FILE-L1-2-0.DLL                        22-08-2013 09:47a  22-08-2013 09:47a      4,608  HA     0x0000EF84     0x0000EF84     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-FILE-L1-2-1.DLL                        22-08-2013 09:47a  22-08-2013 09:47a      4,608  HA     0x00003C1A     0x00003C1A     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-FILE-L2-1-0.DLL                        22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x00008450     0x00008450     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-FILE-L2-1-1.DLL                        22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x00010166     0x00010166     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-HANDLE-L1-1-0.DLL                      22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x0000E8ED     0x0000E8ED     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-HEAP-L1-1-0.DLL                        22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x000021C1     0x000021C1     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-HEAP-L1-2-0.DLL                        22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x0000EAF7     0x0000EAF7     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-INTERLOCKED-L1-1-0.DLL                 22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x0000B23A     0x0000B23A     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.1
    [   ]  API-MS-WIN-CORE-IO-L1-1-1.DLL                          22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x000045ED     0x000045ED     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-JOB-L1-1-0.DLL                         22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x0000D490     0x0000D490     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-LIBRARYLOADER-L1-1-0.DLL               22-08-2013 09:47a  22-08-2013 09:47a      3,584  HA     0x0000BD30     0x0000BD30     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-LIBRARYLOADER-L1-2-0.DLL               22-08-2013 09:47a  22-08-2013 09:47a      3,584  HA     0x0000D4F0     0x0000D4F0     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-LOCALIZATION-L1-2-0.DLL                22-08-2013 09:47a  22-08-2013 09:47a      4,096  HA     0x00007D2A     0x00007D2A     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-LOCALIZATION-L1-2-1.DLL                22-08-2013 09:47a  22-08-2013 09:47a      4,096  HA     0x0000E093     0x0000E093     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-LOCALIZATION-L2-1-0.DLL                22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x00008FA6     0x00008FA6     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-LOCALIZATION-PRIVATE-L1-1-0.DLL        22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x0000E6E5     0x0000E6E5     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-MEMORY-L1-1-0.DLL                      22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x00004D59     0x00004D59     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-MEMORY-L1-1-2.DLL                      22-08-2013 09:47a  22-08-2013 09:47a      3,584  HA     0x0000CDFB     0x0000CDFB     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-NAMEDPIPE-L1-1-0.DLL                   22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x00008D67     0x00008D67     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-NAMEDPIPE-L1-2-0.DLL                   22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x00009B2C     0x00009B2C     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-NAMESPACE-L1-1-0.DLL                   22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x00002953     0x00002953     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-NORMALIZATION-L1-1-0.DLL               22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x00005488     0x00005488     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-PROCESSENVIRONMENT-L1-1-0.DLL          22-08-2013 09:47a  22-08-2013 09:47a      3,584  HA     0x0000E9F5     0x0000E9F5     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-PROCESSENVIRONMENT-L1-2-0.DLL          22-08-2013 09:47a  22-08-2013 09:47a      3,584  HA     0x00010911     0x00010911     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-PROCESSTHREADS-L1-1-0.DLL              22-08-2013 09:47a  22-08-2013 09:47a      4,096  HA     0x000063C2     0x000063C2     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-PROCESSTHREADS-L1-1-1.DLL              22-08-2013 09:47a  22-08-2013 09:47a      4,608  HA     0x00010630     0x00010630     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-PROCESSTHREADS-L1-1-2.DLL              22-08-2013 09:47a  22-08-2013 09:47a      4,608  HA     0x00008162     0x00008162     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-PROCESSTOPOLOGY-L1-2-0.DLL             22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x00007CBC     0x00007CBC     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-PROFILE-L1-1-0.DLL                     22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x0000BD85     0x0000BD85     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-PSAPI-ANSI-L1-1-0.DLL                  22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x00007944     0x00007944     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-PSAPI-L1-1-0.DLL                       22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x0000CF3D     0x0000CF3D     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-PSAPI-OBSOLETE-L1-1-0.DLL              22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x0000C251     0x0000C251     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-REALTIME-L1-1-0.DLL                    22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x00006F45     0x00006F45     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-REGISTRY-L1-1-0.DLL                    22-08-2013 09:47a  22-08-2013 09:47a      3,584  HA     0x00001A30     0x00001A30     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-RTLSUPPORT-L1-1-0.DLL                  22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x0000284A     0x0000284A     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-RTLSUPPORT-L1-2-0.DLL                  22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x000030F5     0x000030F5     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-SIDEBYSIDE-L1-1-0.DLL                  22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x0000BD36     0x0000BD36     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-STRING-L1-1-0.DLL                      22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x0000B628     0x0000B628     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-SYNCH-L1-1-0.DLL                       22-08-2013 09:47a  22-08-2013 09:47a      3,584  HA     0x0000A1F2     0x0000A1F2     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-SYNCH-L1-2-0.DLL                       22-08-2013 09:47a  22-08-2013 09:47a      4,096  HA     0x00005B38     0x00005B38     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-SYSINFO-L1-1-0.DLL                     22-08-2013 09:47a  22-08-2013 09:47a      3,584  HA     0x00008A4D     0x00008A4D     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-SYSINFO-L1-2-1.DLL                     22-08-2013 09:47a  22-08-2013 09:47a      3,584  HA     0x00002200     0x00002200     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-SYSTEMTOPOLOGY-L1-1-0.DLL              22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x0000B88C     0x0000B88C     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-THREADPOOL-LEGACY-L1-1-0.DLL           22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x0000B942     0x0000B942     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-THREADPOOL-PRIVATE-L1-1-0.DLL          22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x00010710     0x00010710     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-TIMEZONE-L1-1-0.DLL                    22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x00001A5F     0x00001A5F     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-UTIL-L1-1-0.DLL                        22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x0000AF6C     0x0000AF6C     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-WINDOWSERRORREPORTING-L1-1-0.DLL       22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x0000234E     0x0000234E     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-WOW64-L1-1-0.DLL                       22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x0000E6CD     0x0000E6CD     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CORE-XSTATE-L2-1-0.DLL                      22-08-2013 09:47a  22-08-2013 09:47a      2,560  HA     0x0000F14E     0x0000F14E     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-CRT-ENVIRONMENT-L1-1-0.DLL                  22-08-2015 07:12p  15-07-2015 07:35a     12,128  A      0x0000B136     0x0000B136     x86  Console    CV,Unknown  0x10000000      Unknown      0x00003000    Not Loaded  10.0.10240.16390  10.0.10240.16390  10.0       12.10       10.0    10.0
    [   ]  API-MS-WIN-CRT-HEAP-L1-1-0.DLL                         22-08-2015 07:12p  15-07-2015 07:35a     12,640  A      0x00004118     0x00004118     x86  Console    CV,Unknown  0x10000000      Unknown      0x00003000    Not Loaded  10.0.10240.16390  10.0.10240.16390  10.0       12.10       10.0    10.0
    [   ]  API-MS-WIN-CRT-RUNTIME-L1-1-0.DLL                      22-08-2015 07:12p  15-07-2015 07:35a     16,224  A      0x0000FE45     0x0000FE45     x86  Console    CV,Unknown  0x10000000      Unknown      0x00004000    Not Loaded  10.0.10240.16390  10.0.10240.16390  10.0       12.10       10.0    10.0
    [   ]  API-MS-WIN-SECURITY-APPCONTAINER-L1-1-0.DLL            22-08-2013 09:47a  22-08-2013 09:47a      3,072  HA     0x0000DFD8     0x0000DFD8     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  API-MS-WIN-SECURITY-BASE-L1-2-0.DLL                    22-08-2013 09:44a  22-08-2013 09:44a      5,632  HA     0x00010828     0x00010828     x86  Console    CV          0x10000000      Unknown      0x00003000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [   ]  KERNEL32.DLL                                           16-07-2014 04:18p  20-03-2014 05:25a  1,036,288  A      0x000FEC4C     0x000FEC4C     x86  Console    CV          0x6B800000      Unknown      0x00140000    Not Loaded  6.3.9600.17056    6.3.9600.17056    6.3        11.0        6.3     6.3
    [   ]  KERNELBASE.DLL                                         16-07-2014 04:18p  19-03-2014 12:43p    836,096  A      0x000D9106     0x000D9106     x86  Console    CV          0x10000000      Unknown      0x000CF000    Not Loaded  6.3.9600.17055    6.3.9600.17055    6.3        11.0        6.3     6.3
    [   ]  LIBRARYLOADER.DLL                                      01-03-2016 07:09a  01-03-2016 06:32a     32,672  A      0x0000FA63     0x0000FA63     x86  Console    CV,Unknown  0x10000000      Unknown      0x0000A000    Not Loaded  6.2.0.1631        0.0.0.0           0.0        14.0        5.1     5.1
    [   ]  NTDLL.DLL                                              16-07-2014 04:25p  03-05-2014 12:09p  1,473,080  A      0x0016DF83     0x0016DF83     x86  Console    CV          0x6B280000      Unknown      0x00168000    Not Loaded  6.3.9600.17114    6.3.9600.17114    6.3        11.0        6.3     6.3
    [   ]  UCRTBASE.DLL                                           22-08-2015 07:12p  15-07-2015 07:33a    901,264  A      0x000E8531     0x000E8531     x86  Console    CV,Unknown  0x10000000      Unknown      0x000DC000    Not Loaded  10.0.10240.16390  10.0.10240.16390  10.0       12.10       10.0    5.1
    [D  ]  EXT-MS-WIN-ADVAPI32-NTMARTA-L1-1-0.DLL                 22-08-2013 09:43a  22-08-2013 09:43a      3,072  HA     0x000075E9     0x000075E9     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-ADVAPI32-REGISTRY-L1-1-0.DLL                22-08-2013 09:43a  22-08-2013 09:43a      3,584  HA     0x00008630     0x00008630     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-APPXDEPLOYMENTCLIENT-APPXDEPLOY-L1-1-0.DLL  22-08-2013 09:43a  22-08-2013 09:43a      3,072  HA     0x00010BF0     0x00010BF0     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-GPAPI-GROUPPOLICY-L1-1-0.DLL                22-08-2013 09:43a  22-08-2013 09:43a      4,096  HA     0x000027B0     0x000027B0     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-KERNEL32-APPCOMPAT-L1-1-0.DLL               22-08-2013 09:43a  22-08-2013 09:43a      3,584  HA     0x000069BB     0x000069BB     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-KERNEL32-DATETIME-L1-1-0.DLL                22-08-2013 09:43a  22-08-2013 09:43a      3,072  HA     0x00005178     0x00005178     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-KERNEL32-ERRORHANDLING-L1-1-0.DLL           22-08-2013 09:43a  22-08-2013 09:43a      3,072  HA     0x0000AAA3     0x0000AAA3     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-KERNEL32-FILE-L1-1-0.DLL                    22-08-2013 09:43a  22-08-2013 09:43a      3,072  HA     0x000012B7     0x000012B7     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-KERNEL32-QUIRKS-L1-1-0.DLL                  22-08-2013 09:43a  22-08-2013 09:43a      3,584  HA     0x0000709D     0x0000709D     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-KERNEL32-REGISTRY-L1-1-0.DLL                22-08-2013 09:43a  22-08-2013 09:43a      3,584  HA     0x0000A1AB     0x0000A1AB     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-KERNEL32-SIDEBYSIDE-L1-1-0.DLL              22-08-2013 09:43a  22-08-2013 09:43a      3,584  HA     0x0000E3AB     0x0000E3AB     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-KERNEL32-WINDOWSERRORREPORTING-L1-1-0.DLL   22-08-2013 09:43a  22-08-2013 09:43a      3,584  HA     0x0000CA04     0x0000CA04     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-KERNELBASE-PROCESSTHREAD-L1-1-0.DLL         22-08-2013 09:43a  22-08-2013 09:43a      4,096  HA     0x0000C32B     0x0000C32B     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-MRMCORER-RESMANAGER-L1-1-0.DLL              22-08-2013 09:43a  22-08-2013 09:43a      3,072  HA     0x0000FD7F     0x0000FD7F     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-NTDSAPI-ACTIVEDIRECTORYCLIENT-L1-1-0.DLL    22-08-2013 09:43a  22-08-2013 09:43a      3,584  HA     0x00006B7B     0x00006B7B     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-NTUSER-STRING-L1-1-0.DLL                    22-08-2013 09:43a  22-08-2013 09:43a      3,072  HA     0x0001010E     0x0001010E     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-SHELL32-SHELLCOM-L1-1-0.DLL                 22-08-2013 09:43a  22-08-2013 09:43a      3,072  HA     0x0000B923     0x0000B923     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    [D  ]  EXT-MS-WIN-SHELL32-SHELLFOLDERS-L1-1-0.DLL             22-08-2013 09:43a  22-08-2013 09:43a      3,584  HA     0x0000B2BD     0x0000B2BD     x86  Console    CV          0x10000000      Unknown      0x00004000    Not Loaded  6.3.9600.16384    6.3.9600.16384    6.3        11.0        6.3     6.3
    
    ************************************| Log |*************************************
    
    Error: At least one required implicit or forwarded dependency was not found.
    
    

  • Dhruvil,

    You are using a newer version of CCS than what this post is about.  In your case, you need to also install the 2015 MSVC redistributable (32 bit version)

    Darian

  • Hello Darian,
    Can you please tell me which exe should i install?
    x64 or x32 as my PC is 64-bit processor.

    Thanks.
  • x32 as CCS is still 32 bit.
    Darian
  • sir, I installed x32 version.But problem still exist
  • Hello Darian,
    I resolved my errors by reinstalling some MSVC redistributables from Microsoft site.
    Actually they were already installed but though some DLL files were missing.
    So i found missing DLL files using dependencywalker software and downloaded missing DLL from opendll.com site.
    And it works!
    Yeah finally i could able to solve my problems.

    And i have to install both x86 and x64 redistributables in order to install some DLL files..

    Any way now i can complete my project.
    And thank you for giving your time suggesting me solutions. In future if i find any trouble regarding my project i will post it in forum and will expect answers from you.

    Thanks,
    Dhruvil Koshti