This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Encountered a problem loading file:



hello,

i am studying how to use CCS 5.5. but when i debug the code, it shows  and then i select proceed, it shows  what should i do now?

  • Hi,

    as the message states, your code unfortunately contains errors.   I would focus on debugging those.

    Best Regards,
    Lisa 

  • Hi, Lisa

    thank you for your reply.

    i found these code on the internet. 

    #include "inc/hw_memmap.h"
    #include "inc/hw_types.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/gpio.h"
    #include "driverlib/interrupt.h"
    #include "inc/hw_ints.h"
    #define SYS_CLOCK        50000000                  
    #define KEY GPIO_PIN_4                              
    #define RED_LED  GPIO_PIN_1            
    #define BLUE_LED GPIO_PIN_2                
    #define GREEN_LED GPIO_PIN_3               
    long key_value = 0;               
    //**********************************************************************
    //**********************************************************************
    void main(void)
    {
            int i = 0;
           long temp = 0;
           
           SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL |
                                  SYSCTL_XTAL_16MHZ | SYSCTL_OSC_MAIN);
          
           SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
            
           GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE,RED_LED | BLUE_LED | GREEN_LED);
            
           GPIOPadConfigSet(GPIO_PORTF_BASE,RED_LED | BLUE_LED| GREEN_LED,
                                     GPIO_STRENGTH_2MA,GPIO_PIN_TYPE_STD);
            
           GPIOPinTypeGPIOInput(GPIO_PORTF_BASE,KEY);
           
           GPIOPadConfigSet(GPIO_PORTF_BASE,KEY,
                                            GPIO_STRENGTH_2MA,GPIO_PIN_TYPE_STD_WPU);
          
           GPIOIntTypeSet(GPIO_PORTF_BASE,KEY,GPIO_RISING_EDGE);
           
           GPIOPinIntEnable(GPIO_PORTF_BASE,KEY);
           IntEnable(INT_GPIOF);
           while(1)
            {
                 
                   if(key_value & KEY)
                   {
                            switch(i)
                            {
                            case 0:
                                    temp =GPIOPinRead(GPIO_PORTF_BASE,RED_LED);
                                   GPIOPinWrite(GPIO_PORTF_BASE,RED_LED,~temp);
                                    key_value&= ~KEY;
                                    i = 1;
                                    break;
                            case 1:
                                    temp =GPIOPinRead(GPIO_PORTF_BASE,BLUE_LED);
                                   GPIOPinWrite(GPIO_PORTF_BASE,BLUE_LED,~temp);
                                    key_value&= ~KEY;
                                    i = 2;
                                    break;
                            case 2:
                                    temp =GPIOPinRead(GPIO_PORTF_BASE,GREEN_LED);
                                   GPIOPinWrite(GPIO_PORTF_BASE,GREEN_LED,~temp);
                                    key_value&= ~KEY;
                                    i = 0;
                                    break;
                            }
                   }
                   else
                   {
                   }
            }
    }
    void KeyISR(void)
    {
           key_value = GPIOPinIntStatus(GPIO_PORTF_BASE,true);

           GPIOPinIntClear(GPIO_PORTF_BASE,key_value);
           SysCtlDelay(10 * (SYS_CLOCK / 3000));
    }
    above all are the codes.
     
    thank you very much

    best regards

    Zhengwei LI
  • Hi,

    unfortunately we are not allowed to debug for you.  What error messages do you get?

    Best Regards,
    LIsa