Other Parts Discussed in Thread: TMS320F28335
Hi,
I am having problems the new compiler for TMS320C28x.
I am using CCS5.5, Device TMS320F28335, Programming Language C++.
Previously I was using Compiler V6.1.5 which is working fine without problems with my source code.
Recently I downloaded the V6.2.3, when I compile the same source code with new one I get following linker error
undefined first referenced
symbol in file
--------- ----------------
___T_10CPwm3Phase ./Source/PwmB6.obj
___T_13COutputBuffer ./Source/Shared/MAX3420.obj
___T_15CCommandHandler ./Source/Shared/MAX3420.obj
___T_4CSpi ./Source/Shared/MAX3420.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "CO3636-3B_Debug.out" not
built
>> Compilation failure
gmake: *** [CO3636-3B_Debug.out] Error 1
gmake: Target `all' not remade because of errors.
I used following Compiler options:
-v28 -ml -mt --float_support=fpu32 --include_path="C:/Program Files/Texas Instruments/C2000 Code Generation Tools 6.2.3/include" --include_path="C:/workspace_v5_5/CO3636-3B/Header" --include_path="C:/workspace_v5_5/CO3636-3B/Header/fonts" --include_path="C:/Projects/TMS320/Include" -g --define=TARGET_F28335 --define=ASSERT_CAN_BREAK --define=LARGE_MODEL --define=_DEBUG --diag_warning=225 --display_error_number --diag_suppress=10063 --diag_suppress=16002 --gen_func_subsections=on
I used following Linker options:
-v28 -ml -mt --float_support=fpu32 -g --define=TARGET_F28335 --define=ASSERT_CAN_BREAK --define=LARGE_MODEL --define=_DEBUG --diag_warning=225 --display_error_number --diag_suppress=10063 --diag_suppress=16002 --gen_func_subsections=on -z -m"CO3636-3B_Debug.map" --heap_size=0x60000 --stack_size=0x380 --warn_sections -i"C:/Program Files/Texas Instruments/C2000 Code Generation Tools 6.2.3/lib" -i"C:/Program Files/Texas Instruments/C2000 Code Generation Tools 6.2.3/include" -i"C:/Projects/TMS320/Lib" --reread_libs --priority --display_error_number --xml_link_info="CO3636-3B_Debug_linkInfo.xml" --entry_point=code_start --ram_model
So I downloaded and tried the other compiler versions V6.2.0 & V6.2.1 but the same story, after that I tried again the old compiler V6.1.5 and it works with V6.1.5 and all older compiler versions.
I checked all the compiler and linker options, compiler and linker paths for libraries, took a look at Linker command files, map file, but couldn't find anything.
I noticed that this error occurs for drived classes for who the base class resides in pre-compiled library, but strangely this error is not appearing with all drived classes, and the code still compiles without errors with Compiler version V6.1.5 and earlier.
I also tried the same, with source code of other projects (based on same device), got the same result (compiles with V6.1.5 and earlier, don't compile with V6.2.x).
Can anyone help me please.
Ishwar