This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

unable to communicate with the emulator in linux

Hello

I want to test some example projects on linux. 

I use EVM C6670 and CCSv5.4.

And I use Ubuntu 12.04 32bit booting program which is located in an external hard disc drive.

 

I rebuild helloworld project and try to launch helloworld.ccxml.

But console printed Error initializing emulator (Error -2083 @ 0x0): Unable to communicate with the emulator.

When I try same example on windows version, it works well.

So I reinstall CCS, but this problem doesn't solved.

What should I do to run projects??

Plz help.