Other Parts Discussed in Thread: TMS320C6657
Path to example project: C:\ti\pdk_C6657_1_1_2_6\packages\ti\drv\exampleProjects\SRIO_LoopbackTestProject
TMDSEVM6657LS
TMS320C6657 Lite Evaluation Module
(with integrated XDS200 Emulator)
Test Connection Window
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\x0208023\AppData\Local\.TI\693494126\ 0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product. This utility will load the program 'bh560v2u.out'. E_RPCENV_IO_ERROR(-6) No connection: emulator was not found Download failed for file C:\ti\ccsv5\ccs_base\common\uscif\xds560v2.out
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06). The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is: An attempt to access the named emulator via USCIF ECOM has failed.
[End]
Consol Window
Error initializing emulator: (Error -2083 @ 0x0) Unable to communicate with the emulator. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.73.0)
I do not know what I need to do.
compiling is completely done. The thing is that there might be some problem in connection.
Please help me!