Hi
I am getting following error:
#10099-D program will not fit into available memory. run placement with alignment/blocking fails
for section ".ebss" size 0x23e9 page 1. Available memory ranges:
TMS320F2808.cmd /LittleRedSBC_sysbios line 107 C/C++ Problem
How to resolve this error?
Following is cmd file extract:
MEMORY
{
PAGE 0: /* Program Memory */
OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
FLASH : origin = 0x3E8000, length = 0x00FF80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Used for "boot to Flash" bootloader mode. */
CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* CSM password locations in FLASH */
ROM : origin = 0x3FF000, length = 0x000FC0 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PAGE 1 : /* Data Memory */
M01SARAM : origin = 0x000000, length = 0x000800 /* on-chip RAM block M0, M1 */
PIEVECT : origin = 0xD00, length = 0x100
L01SARAM : origin = 0x008000, length = 0x002000 /* on-chip RAM block L0, L1 */
H0SARAM : origin = 0x00A000, length = 0x002000 /* on-chip RAM block H0 */
}
/*
* Allocate sections to memory blocks.
* Note:
* codestart user defined section in DSP28_CodeStartBranch.asm
* used to redirect code execution when booting to flash
*
* ramfuncs user defined section to store functions that will be
* copied from Flash into RAM
*/
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASH PAGE = 0
.pinit : > FLASH PAGE = 0
.text : > FLASH PAGE = 0
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASH PAGE = 0,
RUN = L01SARAM PAGE = 1,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart)
csmpasswds : > CSM_PWL PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
/* Allocate uninitalized data sections: */
.stack : > M01SARAM | L01SARAM | H0SARAM PAGE = 1
.ebss : > M01SARAM | L01SARAM | H0SARAM PAGE = 1
.esysmem : > H0SARAM | L01SARAM | M01SARAM PAGE = 1
.cio : > H0SARAM | L01SARAM | M01SARAM PAGE = 1
/* Initalized sections go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASH PAGE = 0
.switch : > FLASH PAGE = 0
.args : > FLASH PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASH PAGE = 0 /* Math Code */
IQmathTables : > ROM PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */
}
Thanks & regards
Newbee