This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

compiler issue in ver 7.3.5

Hi,

I am facing issue in the assembly translation of a structure parsing code on a Turbo Nyquist processor using compiler version 7.3.5

The code bit looks something like this.

 

-----------Global declarations--------

 

typedef struct

{

 

uint16 a;

uint16 b;

uint16 c;

 

}structtype1;

 

typedef struct

{

 

uint16 p;

uint16 q;

uint16 r;

 

}structtype2;

 

structtype1 demo1; // cacheable memory

structtype2 demo2; // cacheable memory

-------------end---------------------------

 

main()

{

                demo1.a = 1;

                demo1.b = 2;

                demo1.c = 3;

 

                Parse_demo2(&demo1);

}

 

Parse_demo2(structtype1* demoptr1)

{

                structtype2* demoptr2 = &demo2;

                cacheWritebackandInvalidate(demoptr2, sizeof(structtype2));

                demoptr2->p = demoptr1->a;                                                                    // line 1

                demoptr2->q = demoptr1->b;                                                                   // line 2

 

                demoptr2->r = demoptr2->p + (demoptr2->q > 0);                          // line 3

                cacheWriteback(demoptr2, sizeof(structtype2));

 

}

 

On executing the code I always see the result to be 0.

On analysing the assembly it is seen that before line 1 and line 2 assignments are completed, line 3 fetches the operands from the memory in line 1 and line 2.