This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code Composer Won't load executables to certain cores

Hi,

I am having very inconsistant results with using CCS on a Windows 7 machine to load programs onto a C6678. More often than not, I can not get CCS to load an executable to the cores I want. I attempt to manage this using the debug configurations menu, and selsecting which core I want to have an executable.

Currently I am attempting to load an SRIO multicore looback example. It will load into Cores 0 and 1, but not 2 and 3. After I attempt to load the programs, Cores 2 and 3 have (running) next to them in the debug window. However there appears to be no code loaded in them.

I have attempted to use the guidance from the following link with no luck. http://processors.wiki.ti.com/index.php/Troubleshooting_CCSv5#Debugger

I have also tried using different C6678 evaluation boards.

Thanks in advance.

  • Hi Dan,

    Please describe in detail how you are trying to load the program in each core (did you create a group? Are you loading one by one? etc). Provide every step. I'm looking for a detailed reproducible test case.

    Screenshot are also useful.

    Also let me know exactly which CCS version you are using? For example, the latest version is CCSv5.5.00077.

    Thanks

    ki