This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS4 Realtime Mode - display needed

All:

I can go into realtime mode on the C2000 by using the Script pull-down. I can also see a variable being updated by selecting that variable and doing "continuous refresh."

However, there are some differences from CCS 3.3 that I think should be noted and some actions to take:

1. CCS 3.3 would have an indicaton at the bottom "bar" stating "polite realtime" - I see no such indication on CCS4.

2. When a variable was changing in "continuous refresh" mode, it would change color to red on CCS 3.3 - there is no such indication on CCS4.

3. In CCS4, when going into realtime mode via the Scripts, the "Generic Debugger Options" page should be updated to show that realtime mode has been entered.

Regards,

Todd Anderson

MCU Apps - Minnesota