Other Parts Discussed in Thread: MSP430G2131
I am using CCS v5.5.0.00077.
I started a new CCS project using the "Hello World" sample with the MSP430G2131 as my target platform. However, the project will not build. I receive the following output to the console:
**** Build of configuration Debug for project sample **** "C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all 'Building file: ../hello.c' 'Invoking: MSP430 Compiler' "C:/ti/ccsv5/tools/compiler/msp430_4.2.1/bin/cl430" -vmsp --abi=eabi --include_path="C:/ti/ccsv5/ccs_base/msp430/include" --include_path="C:/ti/ccsv5/tools/compiler/msp430_4.2.1/include" --advice:power=all -g --define=__MSP430G2131__ --diag_warning=225 --display_error_number --diag_wrap=off --printf_support=minimal --preproc_with_compile --preproc_dependency="hello.pp" "../hello.c" "../hello.c", line 10: remark #1532-D: (ULP 5.3) Detected printf() operation(s). Recommend moving them to RAM during run time or not using as these are processing/power intensive 'Finished building: ../hello.c' ' ' 'Building target: sample.out' 'Invoking: MSP430 Linker' "C:/ti/ccsv5/tools/compiler/msp430_4.2.1/bin/cl430" -vmsp --abi=eabi --advice:power=all -g --define=__MSP430G2131__ --diag_warning=225 --display_error_number --diag_wrap=off --printf_support=minimal -z -m"sample.map" --heap_size=0 --stack_size=50 -i"C:/ti/ccsv5/ccs_base/msp430/include" -i"C:/ti/ccsv5/tools/compiler/msp430_4.2.1/lib" -i"C:/ti/ccsv5/tools/compiler/msp430_4.2.1/include" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="sample_linkInfo.xml" --rom_model -o "sample.out" "./hello.obj" "../lnk_msp430g2131.cmd" -l"libc.a" <Linking> remark #10371-D: (ULP 1.1) Detected no uses of low power mode state changes using LPMx or _bis_SR_register() or __low_power_mode_x() in this project. "../lnk_msp430g2131.cmd", line 93: error #10099-D: program will not fit into available memory. placement with alignment fails for section ".text" size 0x1098 . Available memory ranges: remark #10372-D: (ULP 4.1) Detected uninitialized Port 1 in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins. FLASH size: 0x3e0 unused: 0x3be max hole: 0x3be "../lnk_msp430g2131.cmd", line 96: error #10099-D: program will not fit into available memory. run placement with alignment fails for section ".cio" size 0x120 . Available memory ranges: remark #10372-D: (ULP 4.1) Detected uninitialized Port 2 in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins. RAM size: 0x80 unused: 0x4a max hole: 0x48 error #10099-D: program will not fit into available memory. run placement with alignment fails for section "DATA_GROUP" size 0xf6 . Available memory ranges: >> Compilation failure RAM size: 0x80 unused: 0x4a max hole: 0x48 error #10099-D: program will not fit into available memory. run placement with alignment fails for section "BSS_GROUP" size 0xb2 . Available memory ranges: RAM size: 0x80 unused: 0x4a max hole: 0x48 error #10010: errors encountered during linking; "sample.out" not built gmake: *** [sample.out] Error 1 gmake: Target `all' not remade because of errors. **** Build Finished ****