Other Parts Discussed in Thread: HALCOGEN
Hi,
I'm trying to use CMake to build my project and need some help. I've read the CMake wiki on cross compiling with a tool chain file and seen other people discussing in the forums using CMake, so I'm optimistic that is can be done.
My setup:
CCS v5.4.0 for ARM Cortext R (Hercules RM46)
Ubuntu Linux 12.04
CMake v2.8.12.1
To start, I'm trying to compile some c and asm files from HalCoGen into a library. I invoke CMake with the following results:
cmake -G "Unix Makefiles" -DCMAKE_BUILD_TYPE=debug -DCMAKE_TOOLCHAIN_FILE=../RM46_CCS.cmake ..
-- The C compiler identification is TI 5.0.4
-- The CXX compiler identification is TI 5.0.4
-- Detecting C compiler ABI info
-- Detecting C compiler ABI info - failed
-- Detecting CXX compiler ABI info
-- Detecting CXX compiler ABI info - failed
-- Configuring done
-- Generating done
-- Build files have been written to: /home/michael/ws/workspace/cmake_spike/_debug
When I invoke make, it compiles the c files, ignores the asm files, and tries to link with the following error message:
Linking C static library librm4.a
Error running link command: No such file or directory
If you look at my toolchain file (
set(CMAKE_SYSTEM_NAME Hercules_CCS)
set(HERCULES_PATH /opt/ti/ccsv5/tools/compiler/arm_5.0.4)
# specify the cross compiler
set(CMAKE_C_COMPILER "${HERCULES_PATH}/bin/armcl")
set(CMAKE_CXX_COMPILER ${CMAKE_C_COMPILER})
set(CMAKE_ASM_COMPILER ${CMAKE_C_COMPILER})
set(CMAKE_CXX_LINK_EXECUTABLE ${CMAKE_C_COMPILER})
set(CMAKE_LINKER ${CMAKE_C_COMPILER})
set(CMAKE_STRIP "${HERCULES_PATH}/bin/armstrip")
#ENABLE_LANGUAGE(ASM)
set(CMAKE_AR "${HERCULES_PATH}/bin/armar")
# skip compiler tests
set(CMAKE_ASM_COMPILER_WORKS 1)
set(CMAKE_C_COMPILER_WORKS 1)
set(CMAKE_CXX_COMPILER_WORKS 1)
set(CMAKE_DETERMINE_ASM_ABI_COMPILED 1)
set(CMAKE_DETERMINE_C_ABI_COMPILED 1)
set(CMAKE_DETERMINE_CXX_ABI_COMPILED 1)
# set target environment
set(CMAKE_FIND_ROOT_PATH ${HERCULES_PATH})
# Adjust the default behaviour of the FIND_XXX() commands:
# - search programs in the target environment
# - search headers and libraries in the target environment
set(CMAKE_FIND_ROOT_PATH_MODE_PROGRAM ONLY)
set(CMAKE_FIND_ROOT_PATH_MODE_LIBRARY ONLY)
set(CMAKE_FIND_ROOT_PATH_MODE_INCLUDE ONLY)
# This is a platform definition file for platforms without
# operating system, typically embedded platforms.
# It is used when CMAKE_SYSTEM_NAME is set to "Generic"
#
# It is intentionally empty, since nothing is known
# about the platform. So everything has to be specified
# in the system/compiler files ${CMAKE_SYSTEM_NAME}-<compiler_basename>.cmake
# and/or ${CMAKE_SYSTEM_NAME}-<compiler_basename>-${CMAKE_SYSTEM_PROCESSOR}.cmake
# (embedded) targets without operating system usually don't support shared libraries
SET_PROPERTY(GLOBAL PROPERTY TARGET_SUPPORTS_SHARED_LIBS FALSE)
# To help the find_xxx() commands, set at least the following so CMAKE_FIND_ROOT_PATH
# works at least for some simple cases:
SET(CMAKE_SYSTEM_INCLUDE_PATH ${HERCULES_PATH}/include )
SET(CMAKE_SYSTEM_LIBRARY_PATH ${HERCULES_PATH}/lib )
SET(CMAKE_SYSTEM_PROGRAM_PATH ${HERCULES_PATH}/bin )
Any help would be appreciated to get the asm files compiling and the linker working.
Thanks,
Mike