Other Parts Discussed in Thread: TMS320C6671
When trying to connect to my hardware, a TMS320C6671 DSP, I get the following error.
Error connecting to the target:
Error 0x80000244/-1202
Fatal Error during: Register, Initialization, OCS,
CPU pipeline is stalled and the CPU is 'not ready'. This means
that the CPU has performed an access which has not
completed, and the CPU is waiting. The target may need to be
reset. The user can choose 'Yes' to force the CPU to be 'ready'.
When this is done, the user will have the ability to examine
the target memory and registers to determine the cause of the
CPU stall. If CPU hang is caused by application and it has been
forced to be 'ready', the CPU should not be run without a reset.
Yes - force CPU ready (might corrupt the code)
Disconnect - disconnect CCS so that it can be reset
Retry - attempt the command again
Any suggestion as to what can cause this?