This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I try to import StarterWare package for OMAP L138 LCDK to CCS 5.5.0 in Ubuntu 12.04, 32 bit. The first project was imported successfully. Now, it always shows no project under the fold dialogue box. Please see the screen shot below:
Please help me on this problem. Thanks,
Excuse me. I want to make it clearer. The first project I imported was 'game'. Now, it cannot import any project. I even created another workspace. It fails either.
The path you have selected to search for projects is not where the actual CCS projects are located. The CCS projects are under the "build" sub-directory in the Startware installation, not under "examples".
For the search-directory, specify for example:
C:\ti\OMAPL138_StarterWare_1_10_03_03\build\c674x\cgt_ccs\omapl138\evmOMAPL138\gpio
if you are working with c674x or the equivalent armv5 path if you are working with the ARM.
Hope this helps.