Hello,
When I switch on the cycle counter (Run-> Clock->Enable) for MSP430F2013 on MSP-EXP430FG4618 board or eZ430-F2013 the counter show's an incorrect result on first step: 65,537 on next: 131,087 .... and so on.
If I connect to MSP430FG4618 the cycle counter is working correctly. It seems the SpyBiWire is not working correctly.
The same results are obtained on Windows7 64 bits and Windows XP Professional 32b.
I use a MSP-FET430UIF v1.4a to connect to my experimental board.
By the way- on CCS5.4 the feature worked well.
Best regards,
Juris Sirs