Hi there.
I'm trying to get CCSv6 running on Kubuntu 13.10 64Bit.
(After I tried my best with CCSv5, but that one crashed every time I started a new project)
Installation and all worked well with v6, but if I try to test-upload Code to my Stellaris Launchpad by clicking the Debugger Icon,
CCS complains about missing dependencies.
I could resolve one(libnspr4 by just installing libnspr4:i386),
but resolving the next one (libxpcom.so) didn't work.
I found via apt-file search, that this library is in the thunderbird-dev package,
which I installed (64 and 32 bit) and even linked /usr/libxpcom.so to the thunderbird lib,
but that still didn't work.
Can someone tell me how I can get CCS to find libxpcom?
Thanks,
Christian
Edit: I just tried it with my MSP430 Launchpad and I'm getting no dependency Problems here,
but it can't find the Launchpad (Error initializing emulator: No USB FET was found)
even though I can see it in dmesg([ 4226.570990] hid-generic 0003:0451:F432.0005: hiddev0,hidraw3: USB HID v1.01 Device [Texas Instruments Texas Instruments MSP-FET430UIF] on usb-0000:00:02.1-2.4/input1)