This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can CCS3.3 fully support C5515 ezdsp USB stick ?

Hi,

In the kit disk, it is CCS4.1 provided. But I want to develop C5515 with CCS3.3.

I have searched some time. The support website provides the example projects of CCS3.3.(http://support.spectrumdigital.com/boards/usbstk5515_v2/reva/).This post also seems Ok with CCS3.3. Therefore I thought it may OK using CCS3.3.

However, It seems that CCS3.3 doesn't support XDS100V2 in the following  posts http://e2e.ti.com/support/dsp/c5000/f/109/t/47978.aspx    

http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/46846/167313.aspx#167313

So can anyone tell me the exact answer whether or not CCS3.3 support C5515 ezDSP USB stick.

Thanks.

Chunhai