Other Parts Discussed in Thread: OMAP-L137
Will the CCS Profiler clock work with an ARM9 (such as on the OMAP-L137)? When I enable the Profiler clock CCS pops up this message: Error programming AET Job: There is no AET resource to support this job. If I try to set up the full profiler CCS pops a message that the driver I'm using has no supported activites for this profiling method.
Is it not possible to profile on an ARM target?
*edit* I found a few bug reports detailing a similar problem, but on older versions of CCS: SDSCM00006425, SDSCM00012431. This is occurring in CCS v3.3.82.13