Other Parts Discussed in Thread: CCSTUDIO
I have a CCS 4 problem.
First question: Is there a description somewhere on how to use CCS 4 to load a prebuilt executable onto an EVM board (without having a project etc)?
Main issue: Connecting CCS 4 to the EVM board crashes.
I have a Spectrum Digital DM6437 EVM board. With CCStudio 3.3. I built the NDK helloWorld for that board (packages\ti\ndk\example\network\helloWorld) and everything works. I followed instructions on migrating legacy CCStudio projects and successfully built the new CCStudio 4.0 helloWorld project. I created a target configuration file (attached file: Testing9.ccxml), picking the connection "Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator" and then adding the board "EVMDM6437". These settings seemed closest to the setup that works in CCStudio 3.3. Then I launch this target configuration ... which pops up the transient dialog box "DSK STARTUP Waiting for USB enumeration" (just like CCStudio 3.3) ... and then I am in the debug view (attached file: Screenshot1.png). If I choose "Target->Connect Target" the ide crashes (attached file: DebugServer.dll20100108153359.dmp).
If I use CCS 3.3 to load the helloWorld executable (that was built by CCS 4) it runs fine.
Retry: I cleaned everything (new workspace, new migration of legacy helloWorld.pjt, new Testing9.ccxml) and after the debug view pops up the transient dialog box "DSK STARTUP Waiting for USB enumeration" then the ide crashes (attached file: DebugServer.dll20100108161248.dmp) the difference is that this time I didn't get to try to select "Connect Target". I restarted the ide and exported the error log (attached file: PDEErrorLog.log)
CCS Version: 4.0.2.01003
Code Gen Tools: 6.1.11
DSP/BIOS Version: 5.41.00.06
Reproduce: Import the legacy .pjt file into CCS 4 (attached file: reproduceableTestCase.zip). Delete remaining "helloWorld.pjt" "helloWorld.cmd" "migration.log". Build. Debug (creating Target Configuration).