This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Project template

Hello!

I was wondering if there is a simple way to create a project from a template in CCS4.

My source code structure is as follows:
// Let's call CodeRoot the root of my code tree.
- CodeRoot
- CodeRoot/Common  // Processor independent.
- CodeRoot/Devices    // Processor independent. Some devices, for example BMP150.h / .c for Bosch pressure sensor.
- CodeRoot/x16x         // Folder including routines specific for the x16x series, for instance F1611, F169. Files examples: Uart.c/.h, Coprocessor.c/.h
- CodeRoot/x54x         // Folder including routines specific for the x16x series, for instance F5438. Files examples: Uart.c/.h, Coprocessor.c/.h
- CodeRoot/SB169    // Folder specific to the SB169 board
- Etc.

One project usually includes 6 folders. Everytime, I create a project, I have to add all these folders one by one like this:

Repeat 6 times {
    Project right-click -> new -> folder -> advanced -> brows -> [then a lengthy selection process from Windows root.]
    Now everytime I add a new folder, I have to excludes all its files by default, and add only the parts I need.
}

After this, I have to add the include paths

Repeat 7 times {
    Project right click -> properties -> C/C++build -> Include options -> click the add icon -> [then the same lengthy selection as above, from Windows root.]
}

Note: 7 times, because the path of the project is not included by default.
So I would be happy to have an option to simplify this work. Does anyone have a solution?

Thanks,

Pascal