Hello,
I´ve got the Olimex LPT Programmer on my Windows 7 x64.
When I try to debug the program on my MSP430x1232 or MSP430x5438 (with an Olimex LPT Programmer) with CCS 4.0.1.01001
i get the error message:
Error initializing emulator: Could not initialize device interface.
My LPT configuration: I use a Sunix LPT-PCI extension card with 2xLPT Ports with Vista x64 drivers (seems to work good otherwise)
I suppose it is a bug in CCS 4.0.1.01001, as it was also difficult to get it work with older versions even on Windows XP.
Does anyone have a solution?
Regards,
Tobias