Other Parts Discussed in Thread: OMAP3530
I have created a tool for other ARM9 devices that dump all system registers for a device before. I have done this using brute force register descriptions and hard coded programs to dump register sets to s serial console.
I am looking for a way to automate the generation of an application that can dump registers for new devices by using the XML descriptions of the device it self (in this case OMAP3530) to generate include files that I can build a generic application against to dump device registers to avoid all of the custom work involved with creating such an application.
Is it possible to use CGXML or some other tool chain to walk through these device specific XML files (i.e. ..\ccsv4\common\targetdb\Devices\OMAP3530.XML and other referenced XML files for specific peripheral instances) and generate "C" formatted tables of data that could be used to drive creating a register dumping application that does not require as much custom coding?
Here is an example of the output that my DRA446 register dumping tool produces (brute force code does this); this lists virtual and physical address used running under QNX in this case along with register value and register name (matching documentation names. This has proven to be invaluable because we can actually dump register settings from two different boards and diff the results to find differences in settings. This has allowed us to find customer problems/bugs very quickly in the past...
Jacinto (TMS320DRA446) Register Dumper Version 1.1
-v1
-a
Dumping PLL0 Control Registers
VA: 0x01800C00, PA: 0x01CA1C00
Adr: 0x01CA1C00, Val: 0x0001080D, Reg: PID
Adr: 0x01CA1CE4, Val: 0x00000001, Reg: RSTYPE
Adr: 0x01CA1D00, Val: 0x00000049, Reg: PLLCTL
Adr: 0x01CA1D08, Val: 0x00800000, Reg: SECCTL
Adr: 0x01CA1D10, Val: 0x00000015, Reg: PLLM
Adr: 0x01CA1D18, Val: 0x00008000, Reg: PLLDIV1
Adr: 0x01CA1D1C, Val: 0x00008002, Reg: PLLDIV2
Adr: 0x01CA1D20, Val: 0x00008003, Reg: PLLDIV3
Adr: 0x01CA1D28, Val: 0x00008000, Reg: POSTDIV
Adr: 0x01CA1D38, Val: 0x00000001, Reg: PLLCMD
Adr: 0x01CA1D3C, Val: 0x00000006, Reg: PLLSTAT
Adr: 0x01CA1D40, Val: 0x000001FF, Reg: ALNCTL
Adr: 0x01CA1D44, Val: 0x00000000, Reg: DCHANGE
Adr: 0x01CA1D48, Val: 0x00000003, Reg: CKEN
Adr: 0x01CA1D4C, Val: 0x0000000B, Reg: CKSTAT
Adr: 0x01CA1D50, Val: 0x000001FF, Reg: SYSSTAT
Adr: 0x01CA1D60, Val: 0x00008003, Reg: PLLDIV4
Adr: 0x01CA1D64, Val: 0x00008005, Reg: PLLDIV5
Adr: 0x01CA1D68, Val: 0x00008003, Reg: PLLDIV6
Adr: 0x01CA1D6C, Val: 0x00008005, Reg: PLLDIV7
Adr: 0x01CA1D70, Val: 0x00008016, Reg: PLLDIV8
Adr: 0x01CA1D74, Val: 0x00008000, Reg: PLLDIV9
Dumping PLL1 Control Registers
VA: 0x01800000, PA: 0x01CA2000
Adr: 0x01CA2000, Val: 0x0001080D, Reg: PID
Adr: 0x01CA20E4, Val: 0x00000000, Reg: RSTYPE
Adr: 0x01CA2100, Val: 0x00000049, Reg: PLLCTL
Adr: 0x01CA2108, Val: 0x00800000, Reg: SECCTL
Adr: 0x01CA2110, Val: 0x0000001A, Reg: PLLM
Adr: 0x01CA2118, Val: 0x00008000, Reg: PLLDIV1
Adr: 0x01CA211C, Val: 0x00008001, Reg: PLLDIV2
Adr: 0x01CA2120, Val: 0x00008002, Reg: PLLDIV3
Adr: 0x01CA2128, Val: 0x00008000, Reg: POSTDIV
Adr: 0x01CA2138, Val: 0x00000001, Reg: PLLCMD
Adr: 0x01CA213C, Val: 0x00000006, Reg: PLLSTAT
Adr: 0x01CA2140, Val: 0x000000FF, Reg: ALNCTL
Adr: 0x01CA2144, Val: 0x00000000, Reg: DCHANGE
Adr: 0x01CA2148, Val: 0x00000003, Reg: CKEN
Adr: 0x01CA214C, Val: 0x0000000B, Reg: CKSTAT
Adr: 0x01CA2150, Val: 0x000000FF, Reg: SYSSTAT
Adr: 0x01CA2160, Val: 0x00008002, Reg: PLLDIV4
Adr: 0x01CA2164, Val: 0x0000800B, Reg: PLLDIV5
Adr: 0x01CA2168, Val: 0x00008001, Reg: PLLDIV6
Adr: 0x01CA216C, Val: 0x0000800B, Reg: PLLDIV7
Adr: 0x01CA2170, Val: 0x0000800B, Reg: PLLDIV8
.
.
.