This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code Composer Studio Won't Let Me Create Trial License



Hi, I initially installed CCS with the MSP430 16KB code size limited license. But now, since I want to evaluate the KeyFobDemo, I need a trial license that doesn't have the 16KB limit. The demo produces output larger than 16KB due to its use of Bluetooth libraries and I get the following error when compiling:

Description Resource Path Location Type
#10269 output file "KeyFobDemo.out" exceeds code size limit KeyFobDemo C/C++ Problem
#10010 errors encountered during linking; "KeyFobDemo.out" not built KeyFobDemo C/C++ Problem

I tried to reinstall CCS but it gave me no option to generate a trial license anymore. What can I do to get a trial license?