Hello,
I am building custom board with C6455 and C6713. On TI wiki I found information how to create a driver for CCS 4 and XDS100 to work with C6455. However I have problems to build similar driver for C6713 connection. On the mentioned site it is stated as follows:
"The XDS100 is built on XDS510 technology. Since this is the case, the XDS100 uses the existing XDS510 drivers. So, by default, CCSv4 is shipped with drivers that can be used with any device that works with the XDS510."
Thus I assume that is possible... Can anyone help me to do it ?