There is something I don't understand about the design of XDS100v1.
Below is a partial schematics of the XDS100v1.
The output to T_TCK, T_TMS, T_TDI, T_TRST_N are connected to 74ACT08 (5V supply) through a bus switch with a on resistance less than 22 Ohm maximum for Vcc = 4V. 280x DSP clearly state that the inputs are not 5V tolerance. How can it supports 1.8V or 3.3V DSP? Am I missing something?