This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
C:\Program Files (x86)\Debug JTAG GUI\emulators\
Board_Config\TIXDS100v1.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'Aug 20 2013'.
The library build time was '22:56:19'.
The library package version is '5.1.232.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '4' (0x00000004).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the FTDI FT2232 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for FTDI FT2232 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-183' (0xffffff49).
The title is 'SC_ERR_CTL_CBL_BREAK_FAR'.
The explanation is:
The controller has detected a cable break far-from itself.
The user must connect the cable/pod to the target.
HI HR,
We 1st tried the mini-USB connector on the main EVM. We then tried the USB on the attached XSS560v2 (XDS560v2 Mezzanine daughter card) and the resulting error was the same. Have you seen this issue before with TMDSEV6657 EVM? When we connected to XDS560v2 Mezzanine daughter card, we did try adjusting jumpers J4 and J5 which by default were set to Mini USB and external/Mezzanine Emulator respectively since depopulated.
Hi James,
Do you have the board with the XDS560v2 mezzanine board or with the XDS200, so if you want to use the on board XDS100 than you should remove the mezzanine board (try this) if you want to use the mezzanine board than connect only to the Mezzanine board USB connection,
Thanks,
HR
James,
Have you tried removing the XDS200 mezzanine board and connect to the XDS100 Jtag?
Thanks,
HR
Yes we tried both ways as previously described...connecting to XDS100 Jtag with XDS200 mezzanine board removed as well as connecting to XDS200 mezzanine board. Any additional thoughts and/or settings that we should review in our setup? Have you seen this issue before and if so what are the main causes?
HR,
Any additional input on above. Also, what is link for XDS200 USB driver for PC?
James - What version of CCS are you using? The XDS200 drivers should come with the latest version of CCSv5.
Note that the EVM will default to any external emulator if one is attached (like the XDS200 or XDS560v2 Mezz card). So to use the on-board XDS100v1, you should remove the mezz card (which you already tried).
What is the JTAG connectivity test results when you try to use the mezz card emulator?