This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem selecting version of XDCTools

Hi

I have XDCTools 3.25.0.48 and 3.25.02.70 installed on my build machine.

I want to rebuild my platform using 3.25.0.48, so I selected Window > Preferences > Code Composer Studio > RTSC and set XDCTools version to 3.25.0.48.  I then invoked Tools > RTSC Tools > Platform > Edit View to build the platform, which was reported as successful.

However, when I look at .xdcenv.mak I see:

override XDCROOT = C:/ti/xdctools_3_25_02_70

so it seems that the platform was built with 3.25.02.70, which is incompatible with my project.

Why isn't CCS using 3.25.0.48?

Best regards

David