This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux CCS 5.5.0 refuses to change its port number



Hi,

I am using CCS 5.5.0 on Linux Ubuntu 12.04, 32 bit. The project is L138 LCDK on RSE mode. When I  create a connection with the target. The first two connections are correct. I don't know what reason it cannot connect to the target. The problem is that CCS always add port number to the host, no matter I switch it back to default (grayed).

The port number is always 22, even after I temporary set it to 333 intentionally and back to default.

At the beginning, I realized that this port can introduce an sshd error. I corrected it, the two connections were right. Later, it began to pop this extra port error. Anyone can help?

Thanks,

  • When I connect to the target in a terminal, it also has the same problem:

    robert@Aspire-M5100:~$ ssh root@192.168.0.131
    ssh: connect to host 192.168.0.131 port 22: No route to host

    At the far beginning, I ran the above command in a terminal too. There was no such problem. I don't know what introduces such errors.

    BTW, I would like to post the detail message of previous window below.

  • Hi,

    I was able to change the port without problems (I did not connect as my Linux systems are partially down at the moment). Can you confirm if you are able to change this by clicking on the (very) small button right beside the port box parameter?

    Hope this helps,

    Rafael