Hello,
My first question is, when looking at the properties for a project, the command for the MSP430 Compiler and Linker reference "${CG_TOOL_CL}", but I am unable to find where this variable is set at. Under the Resource -> Linked Resources there are a few Path Variables that are define (e.g., CCS_BASE_ROOT), but the variable CG_TOOL_CL is not defined. Where is this located at?
The second, right now I am using the Windows GUI to build the project though eventually this needs to be script driven from a Linux environment. Where would I find information on how to build/convert my existing project to be built within Linux??
Thanks and regards,
Mark