Other Parts Discussed in Thread: TMS320F28335, CONTROLSUITE
Hello
1) I setup CCSv5.5 (offline install), and update C2000 compiler to version 6.2.4 - succesfull.
2) I try update emulation packages, but, after restart CCS, see error:
ZIP-file:
0882.60556FE5-C1A1-4061-8DF8-FFB8393BAE2D.zip
After updating error CCSv5.5 believes that all elements are installed correctly because does not display them in the list of available updates.
Prior to this project collected CCSv5.4 compiler C2000 v2.1.6, JTAG SAU510-USB Iso Plus. The project is running on the target board processor TMS320F28335. Decided to switch to CCSv5.5.
Removed CCSv5.4, drivers JTAG SAU510-USB Iso Plus.
Set CCSv5.5, new drivers SAU510-USB Iso Plus and controlSUITE supporting CCSv5.5, updated and what I can get , except for the above problemmy :
1) Compiler Error
Console text:
**** Build of configuration Release DZT for project BM02 **** "C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all 'Building target: bmdzt02.out' 'Invoking: C2000 Linker' "C:/ti/ccsv5/tools/compiler/c2000_6.2.4/bin/cl2000" -v28 -ml -mt --float_support=fpu32 -g --define="LARGE_MODEL" --define="_RELEASE" --undefine="_DEBUG" --quiet --verbose_diagnostics --diag_warning=225 --issue_remarks --asm_listing --output_all_syms --cdebug_asm_data -z -m"bmdzt02.map" --stack_size=0x200 --warn_sections -i"C:/ti/ccsv5/tools/compiler/c2000_6.2.4/lib" -i"C:/ti/ccsv5/tools/compiler/c2000_6.2.4/include" -i"D:/Work/23DZT/NP/BM02" -i"C:/TI/controlSUITE/device_support/f2833x/v133/DSP2833x_common/lib" -i"C:/TI/controlSUITE/libs/math/IQmath/v160/lib" -i"C:/TI/controlSUITE/libs/math/FPUfastRTS/V100/lib" --reread_libs --priority --verbose_diagnostics --issue_remarks --xml_link_info="bmdzt02_linkInfo.xml" --entry_point=code_start --rom_model -o "bmdzt02.out" -l"rts2800_fpu32_fast_supplement.lib" -l"rts2800_fpu32.lib" "./doc/Проекты ЦП/Актобе проект/БКЖР?.656326.036-03.04 Р‘РРњРџ-ДЗТ.3.obj" "./source/system.obj" "./source/exchange.obj" "./source/caskad.obj" "./source/calc.obj" "./source/bmdzt02.obj" "./source/EnDisInterrupt.obj" "./source/DSP2833x_PieVect.obj" "./source/DSP2833x_DefaultIsr.obj" "./source/DSP2833x_CodeStartBranch.obj" "./stsource/DSP2833x_usDelay.obj" "./stsource/DSP2833x_GlobalVariableDefs.obj" "./stsource/DSP2833x_ADC_cal.obj" "../lib/IQmath_fpu32.lib" "../cmd/DSP2833x_Headers_nonBIOS.cmd" "../cmd/F28335_DZT.cmd" "../cmd/dpramDZT.cmd" -l"IQmath_fpu32.lib" INTERNAL ERROR: C:/ti/ccsv5/tools/compiler/c2000_6.2.4/bin/cl2000 aborted This is a serious problem. Please contact Customer Support with this message and a copy of the input file and help us to continue to make the tools more robust. gmake: *** [bmdzt02.out] Error 2 gmake: Target `all' not remade because of errors. **** Build Finished ****
2) Error when trying to debug :
Error connecting to the target:
(Error -203 @ 0x0)
The test bus controller is not compatible with the installed software.
(Emulation package 5.1.232.0)
I ask to specify which versions CCSv 5.x and С2000 build tools configuration can now be used to complete the development of software for the specified TMS320F28x35.
Or get a recommendation on the application CCSv 5.5 - installation and tuning for bugs described.