CCSv5.5.0.00077
My compiler errors are not being reset after a successful build. Any idea what could cause this? Is this a known bug?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mike,
do you only see this if you get a "nothing to make"? I just tried to reproduce this, by introducing an error and then removing it and for me the problems view cleared.
Could you send further details or perhaps a screen capture?
Best Regards,
Lisa
I believe it might have something to do with the number of source files. Attached is a test case with 256 source files.
- Clean and build
- Change function name in in func000.c from func000() to funcnnn() to cause a linker error.
- Build. There should be a linker error.
- Change name funcnnn() back to func000().
- Build. Should be successful. Prior linker error still there. Attempt to run the app will cause warning about the "error".
Lisa,
Lisa TI said:in your project files/folders you should notice the .metadata, you may simply delete it.
This recommendation should come with a very emphatic warning that all of your previous project will have to be re-imported, and that all of your customized settings will be wiped out. Depending upon your workspace complexity, this could cause quit a bit of re-debugging :(
FYI, the above did NOT fix the problems I am seeing. I have narrowed the non-reset errors to memory allocation errors in the linker .cmd file (text editing errors ARE reset). Please try to create a memory allocation error, then fix it and see whether your errors get set. I created the allocation error below, then fixed it, compiled with no reported errors, but (as the screenshot show) the error indicator was not reset.
Also FYI, even when the compiler gives NO errors, the left-over, non-reset errors will trigger a warning that you are attempting to debug a file with errors when you attempt to debug the non-errored .out file.