This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using the MSP-FET430UIF on CCE V3 after installing CCS V4

I recently installed CCS V4. I have legacy projects in both CCE V3 as well as IAR Workbench V5. After upgrading, I cannot use my MSP-FET430UIF. I get a

"failed to initialize device" in IAR

and

"An exception occurred! Type:RuntimeException,.....entity could not be opened. ID=...TIMSP430-USB.xml" in CCE.

I've tried uninstalling the serial drivers and using the IAR or CCE and still get the same errors. I'm not as concerned with the CCE problem, but I have a licensed version of IAR Workbench and need this to work. Has anyone run into this problem before and how did you solve it. Any help is appreciated.

 

Nick

  • Nick,

    Try backing up the msp430.dll in IAR Workbench and copy in the one from CCSv4.  The CCSv4 version of the file is in \ccsv4\DebugServer\Drivers

    John

  • John,

     

    Thanks! That did the trick!

     

    Nick

  • Hi,

    I don't understand WHY this trick really Works on CCSV4 ( 4.0.2 ) with board ez430-RF2500 ( 2008) .

    If you change the msp430.dll file version 2.4.1.4  to msp430.dll file version 2.3.3.0 you not more receive the message of CCSV4 like : - Error initializing emulator: Could not communicate with FET.

    You can work too with an IAR IDE together with CCSV4.

    Hey TI's Guys! What's happen with compatibilities?


     

  • I too am experiencing this same issue and love that a workaround has been discovered.  

    The trouble is, I don't have (and have looked for high and low on the Internet) the older MSP430.dll and HIL.dll

    My understanding is that I need those DLLs from slac050r.zip which contains FET_R511.exe

    Where can I find either the zip, the contained exe, or the actual dlls I seek?

    Thanks!

    -kP

  • Hi,

    The DLLs are here,  from FET_R511.exe ( TI Development tool IAR eZ430 - 2008 )

    link : http://rapidshare.com/files/320345521/DLLs_from_FET_R511.rar.html ( msp430.dll and hil.dll - 14/2/2008)

    ( But, I think that you need only one dll, to CCSV4 works (Hdd:\ccsv4\DebugServer\drivers\msp430.dll))

    enjoy,

    FNTN