This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS4 hangs up at switching of lay-out of keyboard

At the change of lay-out of keyboard (Ctrl-Shift or Alt-Shift) there is a stop of work of editor for a time to 40 seconds.

 

  • Hi Eduard,

    This is a known issue. See: http://tiexpressdsp.com/index.php/Language_Pack_Installation under Known Issues. It is currently under investigation.

    Thanks

    ki

  • I do not use a language packs

  • While it is under the "Language Pack" topic, the issue itself is not related to it. You are using the Language Bar in Windows and switching languages/encoding, correct?

  • I use Windows XP Sp3 Eng with switching between the Russian and English languages. Switching of language is in the window of editor CCS4 by a keyboard or mouse on Language Bar results in the stop of work CCS4 on 40-45 seconds. In a title bar CCS4 a report appears "Not responding". After it there is work of the program CCS4 recommences.

  • Taken from a site eclipse.org CDT 6.0 works without the indicated error.

  • Yes the issue appears to be specific to CCSv4 (or the CDT version CCSv4 uses).

    ki

  • Creates a problem Internet Explorer 8. Its delete does not give an effect. CCS4 it is needed to put on Windows XP Sp3 with Internet Explorer 6 - then all works correctly.

  • A problem is corrected in a new release from 10 September.

  • New version CCS 4.0.2.01002 now hangs up - now even versions will droop and odd it is not

  • New version CCS 4.0.2.01003 now hangs up

  • Hi Eduard, 

    Could you provide more information on the hang in CCS v4.0.2? Which OS are you using, system specs, how long is the hang? Maybe attach a screen capture of CCS main window when you initiate keyboard layout switch. Does it hang when you switch from Russian to English, English to Russian or both?  Does it make a difference if you use a different keyboard? 

     

    Thanks,
    Martin

     

  • I test CCS 4 under Windows XP and Internet Explorer 8. At switching of keyboard layout with English on Russian and back there is a stop of operation of editor CCS for the period of 45-45 seconds. It was in versions 4.0.0 and 4.0.2.01002. Version CCS 4.0.1.01001 works normally. The last version 4.0.2.01003 at layout switching hangs up for indefinite time. For version 4.0.0 the reason such the behaviour was presence in system of Internet Explorer 8.

     

  • Hello Eduard and others.

    I have the same problem. I use Windows XP SP3, pre-SP4 and Code Composer Studio ver 4.02.01003.   I have 1.3Gb RAM.

     At  any switching of keyboard layout with English on Russian and back there is a permanent stop (hang up) of operation of editor CCS.   Or at  any  switching language in Language Bar CCS editor hang up too.

    Is there any problem solving at present moment?

     

    Thanks.

     

     

  • Проблема существует еще с версии 4.0, в 4.0.1 вроде как исправили - по крайней мере она у меня в "транс" не впадает под Windows XP SP3 + IE8. Версию 4.0.2 тестил на VMware c Windows XP SP3 + IE8. Когда разбирался с глюком в 4.0 выяснил что под ХР именно ИЕ8 является причиной появления тормозов - его снос уже не помогает. У моих знакомых подвисала при переключении раскладки и 4.0.1. Пробовал свежие эклипсы сдт - они такой глюк не имеют. Не думаю что разработчики будут править такой глюк - англичанам раскладку переключать не нужно. Попробуй написать в службу поддержки - но от них к сожалению толку бывает мало.

  • Жаль, что у Вас сложилось такое мнение о службе поддержки. Она помогает в 95% случаев и только в исключительных случаях инженер не в силах помочь заказчику сразу. Надеемся, что Вы продолжите обращаться в центр поддержки и убедитесь что "толк" в этом есть. Наши коллеги осведомлены об этой ошибке и надеемся, что вскоре поступит возможное решение проблемы.

    Если у Вас появится дополнительная информация по этому поводу, сообщайте нам.

     

     

  • Добрый день!

    Эдуард, благодарю за отклик на сообщение.

    Александр, очень надеюсь на скорое решение этой проблемы.  Потому что она добавляет массу неудобств в написании программ на CCS.

    Как я уже написал выше  - у меня после переключении раскладки клавиатуры или после смены языка ввода происходит вечное зависание CCS. Причем у меня одинаково зависают как CCS 4.01 так и версия 4.02.

    И из-за этого приходится полностью отключать возможность смены раскладки или языка ввода в Windows, чтобы случайно не завесить ПО и не потерять весь набранный текст.

     

  • I managed to adjust normal operation of version 4.0.2 on VMware with WinXP by the following operation - flag turnings the power on and off "Extend support of advanced text services to all programs" in "Control Panel\Regional and Language Options\Languages\Details\Advanced" with reboot of system after each change of a state of a flag.

    Мне удалось наладить нормальную работу версии 4.0.2 на VMware с WinXP путем следующей операции - включения и выключения флажка "Extend support of advanced text services to all programs " в Control Panel\Regional and Language Options\Languages\Details\Advanced с перезагрузкой системы (после каждой смены состояния флажка). На основной системе версия 4.0.1 работала нормально и после обновления через интернет на 4.0.2 ничего плохого не произошло. Кстати пишу это сообщение в ИЕ8 и переключение с русского на английский удается сделать только мышкой на тулбаре - судя по интернету проблема широко известная, скорее всего они как то связаны - так как проблема в композере возникает только после установки ИЕ8 - скорее всего он как то включает расширенную поддержку языка но в контрольной панели это не отображается.

  • К сожалению, мне это шаманство не помогло. Кстати, обсуждение на эту же тему есть еще по ссылке http://e2e.ti.com/ru/forums/t/59.aspx

  • Я связался коллегами из Европейского тех. отдела и мне сообщили, что за этим форумом уже следит один из лучших инженеров, но понимает только по английски. 

    Alexandr Danilov said:

    Кстати, обсуждение на эту же тему есть еще по ссылке http://e2e.ti.com/ru/forums/t/59.aspx

    В этой связи, прошу все советы на русском языке размещать именно там.

    Благодарю за понимание

  • Hi Eduard!

    I use your methode:  "I managed to adjust normal operation of version 4.0.2 on VMware with WinXP by the following operation - flag turnings the power on and off "Extend support of advanced text services to all programs" in "Control Panel\Regional and Language Options\Languages\Details\Advanced" with reboot of system after each change of a state of a flag."

    And now my CCS v4.02 doesn`t  halt at all !  Now after each language switching  there is no any pause in CCS work.

    Thank you!

  • Yes, much thanks to Eduard for finding this workaround! We have validated that it does work in our environment.

    And FAQ for this has been added to the CCSv4 FAQs:

    http://tiexpressdsp.com/index.php/FAQ_-_CCSv4#Q:_How_to_prevent_CCS_from_locking_up_when_changing_languages.3F

    Thanks again

    ki

  • Hi Ki !

    In FAQ there is a little inaccuracy as I think. FAQ writtes:

    "If you change the Windows language setting while running CCS it is possible to hang CCS. There is a fix in CCSv4.0.2 and later to help with this however if you still experience the problem you may need to adjust a setting in Windows XP. Go to Control Panel -> Regional and Language Options -> Languages -> Details -> Advanced. Turn on the option for "Extend support of advanced text services to all programs".  

    But in my case if I turn ON option "Extend support of advanced text services to all programs" and reload computer  it cause CCS v4.02 halt after language changing.  It only work if this option is turn OFF.

    Initially I have option "Extend support of advanced text services to all programs" in turn OFF state and have problem with CCS halting.  So I need to turn ON option, after reload Windows, after that turn OFF option and reload WinXP too.  And only after that my CCS4.02 start working properly.

    And Eduard wrote the same:

    "I managed to adjust normal operation of version 4.0.2 on VMware with WinXP by the following operation - flag turnings the power on and off "Extend support of advanced text services to all programs" in "Control Panel\Regional and Language Options\Languages\Details\Advanced" with reboot of system after each change of a state of a flag."

    Thanks

  • One more additions:

    In FAQ written: "There is a fix in CCSv4.0.2  ...... ".

    So as I understand there is no fix of this problem in CCS4.01 and CCS4.02 versions.

  • That's very interesting because for me, that option was in the OFF state but when I turned in ON and the restarted, the issue was gone (I did not have to turn it OFF again). I checked my option just now and it is still ON.

    In regards to the 4.0.2 comment, there were some fixes made that help resolve some other related issues and that is what that comment refers to.

    Thanks

    ki