This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

vmlinux symbol file error

Other Parts Discussed in Thread: OMAP-L138, AM1808

Hi,

I'm using OMAP L138 with jatag xds510 usb

I use ccs v4 to connect the target and load symbol...

But there is an error when i try to enable the OS debuging. (Shown below)

Error: "ARM9_0: Can't initialize TLD Device Driver: A supported Linux image is not detected on the target: No kernel symbols are detected. Please load the vmlinux symbol file and try again."

The image that i build is from Linux windriver (ealf)

Do I need todo any setting ifi use this kind of image?