CCSv5.5, C5515
I have created two different linker command files with differing memory allocations. When I change the selection of the desired linker command file in my project directory using Project ->Properties->Linker Command File->Browse, sometimes the correct .cmd file is shown to be active in my project tree. Other times both linker cmd files are shown as "excluded from build". At this point, neither .cmd can be selected by browsing to their location. Is this a bug?
Also, if you select from the drop down list of available linker files, it is impossible to determine the path of the files since they have the same file name as my custom c5515.cmd file.