Other Parts Discussed in Thread: CCSTUDIO
Hi,
How can I add a *.dll library file to my project i CCSv3.1
Thanks,
Jarek
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CCSTUDIO
Hi,
How can I add a *.dll library file to my project i CCSv3.1
Thanks,
Jarek
Hi,
I want to compute 384-point FFT (I can't use standard libraries because they use radix-2 algorithm), so I try to add libfftw3-3.dll from www.fftw.org.
Jarek
Hi,
I add libfftw3-3.dll under the linker (Incl. Libraries (-l) ) and when I try rebuild my project I have the following errors:
[Linking...] "C:\CCStudio_v3.1\C6000\cgtools\bin\cl6x" -@"Debug.lkf"
<Linking>
>> libfftw3-3.dll, line 1: error: illegal input character: hex ffffff90
>> libfftw3-3.dll: error: system error, can't open file 'MZ.obj' for input: No
such file or directory
>> Compilation failure
Build Complete,
3 Errors, 0 Warnings, 0 Remarks.
Jarek
Jarek,
Sounds to me that you are taking a pre-compiled windows dll and trying to include it in a CCS project. That will never work, dll was probably generated using a completely different compiler. You need to take FFTW source code and use TI compiler (which should be part of CCS) to generate a library file. You can then use that library in your CCS project. FFTW FAQ's have some basic information on this(i.e. source code conforms to ANSI-C and any decent compiler should be able to generate a library).
Martin