This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F280x flash lock during erase

Hi,

I am having problems with the flash being locked during flash operations, without the password protection being deliberately activated by me.

I am using CCS4.0.2 (upgraded once), Blackhawk USB2000 emulator and F2808 ControlCARD in an experimenter's dock.  I recently bought this hardware, but have many previous years experience with CCS3.x, Spectrum Digital 510usb emulator and F281x.

The first time it happened, I tried to write a simple project to flash.  I made sure that the password protection was not set - password bits all ones in CSMPasswords.asm.  The programming sequence stalled, and after starting the IDE again the flash was locked.  After that I had to order more ControlCARDs and did development work for a couple of weeks using RAM only with no problems.

The second time it happened (now), I wanted to program to flash because the code size was getting close to the RAM size limit.  I tried to play it safe.  I opened a debug session, and opened the On-Chip Flash tool.  I tried using this tool to erase flash bank A only, but it reported that there was an error erasing the flash.  The flash was still unlocked.  I tried two more times, after which it reported that the flash was locked or the device not connected.

I'm not sure if this is a software or hardware problem.  Any thoughts would be appreciated.

Thanks in advance,

Douglas

ps - I'm just wondering whether the flash circuitry draws an impulse of current when a flash erase operation starts, and whether this might cause a catastrophic supply voltage dip if the external supply is weak?  I'm down to my last ControlCARD and am loathe to sacrifice it to find out!!