GUI Composer 5.5 is packed with a TI-logger.dll file. (logging grid widget into array functions?)C:\ti\guicomposer\ccs_base\emulation\analysis\bin\ofs
Can logging of the scalier grid (graphs) widget link into local computers file system (Promised Feb.2013) exporting data directly into an MS-Excel CSV file? One can set the INPUT widget characteristic type = file.
If not is there a DSS method able to hook the TI-logger.dll for use in the grid widgets or is there some easier way to accomplish the same function in java script or more simply in HTML5?
We have reviewed EK-LM4F232 RDK which includes C++ logger GUI.exe, the source files missing library directories cause compiler errors using Cygwin C++ compiler. That alone making GUI composer the winner at this time.