This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is there any public documentation for GTI functions



When turning on debug server logging to try and attempt to debug problems such as EXPKITOMAPL138_ARM.gel script from CCS 5.5 reports errors writing to target the logging reports the parameters at entry and exit from GTI functions, along with the function return status.

Are there any public documents which describe the GTI function API, or that that proprietary information only available to Emulator manufacturers?

If I knew what the GTI function API was, it would make trying to debug / create a re-producible test case simpler.

  • Hi Chester,

    Chester Gillon said:
    Are there any public documents which describe the GTI function API, or that that proprietary information only available to Emulator manufacturers?

    As you suspected, it is not something we have publicly available. You would most likely need to request access to it and there would be legal stuff involved (NDAs to sign, etc). 

    It is best to simply send the logs to us so that the debug server engineers can take a look. They can decipher them.

    Thanks

    ki