This problem has been reported in the past (http://e2e.ti.com/forums/p/7471/30223.aspx#30223 by Edward) but probably hasn't been addressed by TI (possibly it was difficult to replicate).
When openiing Project->Properties->C/C++ Build: all the tabs for Configuration Settings (Tool Settings, Build Settings etc.) are completely missing. Left pane of the dialog box has to be resized to have all missing elements appear on the screen. In my case (as in Edward's case - see thread mentioned above) this problem demonstrates itself only on Vista64. Similar problem exists with dialog box for setting up target configuration. The problem is seemingly minor because solution is simple (resize every time left pane), but it can be quite time consuming if one doesn't know about it. Nothing about it is mentioned in FAQ and there is no separate thread for GUI problems on this forum. Not knowing what's going on I unistalled CCS and reinstalled it again, which takes time for full version and then I installed it again on XP to find out that everything works OK there. I'm running CCS Version: 4.0.2.01003 on Vista Businees 64 SP2.