Hi all,
I'm using the C6416 DSK (720MHz) with CCS3.3, I have installed the USB driver and run the SD test on the board which passed, when I'm trying to connect to the board I'm getting the Error -
"Error initializing emulator
I/O Port = 540
Board Name: C6416 Revision 1.1 DSK
Cpu Name: CPU_1"
What can be the issue?
Many Thanks,
HR